2025-08-01 1:20 AM - edited 2025-08-01 1:22 AM
Hi,
I am using STM32Cube_FW_H5_V1.5.0.
I initialize a MPU region with the following code, using only LL-calls:
LL_MPU_ConfigRegion(LL_MPU_REGION_NUMBER6, LL_MPU_REGION_PRIV_RW|LL_MPU_INSTRUCTION_ACCESS_DISABLE|LL_MPU_ACCESS_NOT_SHAREABLE, LL_MPU_ATTRIBUTES_NUMBER2, 0x90000000U, 0x9FFFFFFFU);The corresponding MPU register MPU_RLAR_Ax gets set to 0x9FFFFFE3, wich is obviously wrong because I wanted to select attribute#2 and instead the attribute field gets set to 0x1.
For verification I did the same initialization using HAL-calls:
MPU_Region_InitTypeDef region;
region.Enable = MPU_REGION_ENABLE;
region.Number = MPU_REGION_NUMBER6;
region.AttributesIndex = MPU_ATTRIBUTES_NUMBER2;
region.BaseAddress = 0x90000000U;
region.LimitAddress = 0x9FFFFFFFU;
region.AccessPermission = MPU_REGION_PRIV_RW;
region.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
region.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
HAL_MPU_ConfigRegion(®ion);Now the MPU register MPU_RLAR_Ax gets set to the correct value of 0x9FFFFFE5.
I think the bug is within the LL_MPU_ConfigRegion() code. The current implementation of this function in fw1.5.0 is:
__STATIC_INLINE void LL_MPU_ConfigRegion(uint32_t Region, uint32_t Attributes, uint32_t AttrIndx, uint32_t BaseAddress,
uint32_t LimitAddress)
{
/* Set region index */
WRITE_REG(MPU->RNR, Region);
/* Set region base address and region access attributes */
WRITE_REG(MPU->RBAR, ((BaseAddress & MPU_RBAR_BASE_Msk) | Attributes));
/* Set region limit address, memory attributes index and enable region */
WRITE_REG(MPU->RLAR, ((LimitAddress & MPU_RLAR_LIMIT_Msk) | AttrIndx | MPU_RLAR_EN_Msk));
}where line 11 should be changed to:
WRITE_REG(MPU->RLAR, ((LimitAddress & MPU_RLAR_LIMIT_Msk) | (AttrIndx << 1) | MPU_RLAR_EN_Msk));
}A change of the LL_MPU_ATTRIBUTES_NUMBERx definitions might be another option to solve this, but might have a major impact on the rest of the firmware pack since these definitions are used in a lot of places.
Thank you very much for confirming this bug. If it is a real bug and not a miss-interpretation on my side I would be very happy to see it fixed eventually.
Best Regards
Thomas
Solved! Go to Solution.
2025-08-01 2:44 AM
Hello @TThan
Thank you for reporting this point. An internal ticket is created in order to investigate and fix this potential defect (ticket number 215184)
With regards
2025-08-01 2:44 AM
Hello @TThan
Thank you for reporting this point. An internal ticket is created in order to investigate and fix this potential defect (ticket number 215184)
With regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.