2025-07-01 5:18 AM
Hello ST Team,
I am currently working with the STM32U5 Discovery board (B-U585I-IOT02A) to connect to Azure IoT Central, and I’ve tried two different approaches. I'm facing two distinct issues in each method, as described below:
Reference: https://www.youtube.com/watch?v=BZn2PCvgL9s
The video references a specific GitHub repository for the Azure connection demo, but the repo is currently unavailable .
I proceeded using the latest available X-CUBE-AZURE package from the official ST GitHub.
When I run the project on my B-U585I-IOT02A board, I get the following runtime error: STM32U5_TrustZone_Disable
This seems to be a TrustZone configuration mismatch between the project and the board
Reference: https://community.st.com/t5/stm32-mcus/how-to-quick-connect-stm32u5-to-azure-iot-central/ta-p/49685
I followed the ST community Quick Connect guide.
Wi-Fi connects successfully to my access point.
However, the board fails to resolve the Azure endpoint with the error: DNS create fail
When I re-run the application, I receive: Invalid SPI Type ef
Request:
What is the correct TrustZone setting required for the latest Azure Quick Connect examples?
Could you share or restore the GitHub repo referenced in the YouTube video
What could be causing the DNS create fail even after successful Wi-Fi connection?
How can I properly reset or reinitialize the SPI interface to avoid Invalid SPI errors?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.