2024-01-16 5:11 PM
Hi Folks,
I'd like to find an example of accessing a USB drive using the STM32CubeIDE. I'm currently using the Nucleo-H7A3Zi-Q board.
I believe I have setup the hardware correctly using the device configuration tool but I can't seem to find a simple or concise example on how to develop the code.
I have downloaded the STM32Cube_FW_H7_V1.11.0 code and examples but it still seems more complicated than it should. I've looked at STM32Cube_FW_H7_V1.11.0\Projects\NUCLEO-H7A3ZI-Q\Applications\USB_Host\MSC_Standalone\ but I don't understand how (or what) to import into my workspace.
For a start I just want to be able to write a "Hello World" into a file on the USB key.
Anybody have a good tutorial or example I can use?
Thanks,
Richard
2024-01-17 2:00 PM
I do have another question - Where does the following code belong:
if(usb_status>0) // if usb mounted
{
fresult = f_opendir(&dir,USBHPath); // main dir open
fresult = f_readdir (&dir, &file_info);
}
Does it go before or after the case statements?
if(Appli_state == APPLICATION_READY && usb_status == 0)
2024-01-17 2:02 PM - edited 2024-01-17 2:02 PM
TRY...debug.. breakpoints at f_mount , and opendir -> see fresult ok ? (= 0 ) ... ???
2024-01-17 2:16 PM - edited 2024-01-17 2:18 PM
Hmmm.. the Appli_state ... is , what the usb telling us. Not more. ( at end of while loop, after
/* USER CODE BEGIN 3 */ , as i showed. )
Then in main, in the "while" loop, we wait (do ...nothing or something..) until usb is ready.
So i use here: "if mounted" -> then we can read or do more , before its mounted (maybe 100ms or so) any access would be useless, crash or at least some error. -> in main while(1) loop then !
2024-01-17 2:16 PM
usb_status = 0
Appli_state = APPLICATION_IDLE
fresult = FR_OK
2024-01-17 2:20 PM
After I step thru the while() loop a few times the Appli_state changes to APPLICATION_READY. But it never changes from that.
2024-01-17 2:26 PM
First : debug.. breakpoint at f_mount ; if connect to stick, you landing here . Then mount should work also.
If not ...check your hardware : is usb stick there? is 5V at the plug ? (i dont know...i dont have this board, just my own boards); see circuit of your board, maybe this "activate vbus.." is wrong, or the PF10 (enable vbus) not switches 5v to the plug, or need a jumper setting...is 5V there ?
2024-01-17 2:31 PM
Aaa...you should not "step" the while loop, this usb thing needs enumeration and so on...complex...it will need many times call the usb_host process, so dont break this processing. We only look for the result, just run and use breakpoint at ...mount . If it not coming there, then we look, why.
2024-01-17 3:03 PM
OK, I removed the breakpoint and just let it run for a minute and then I inserted the breakpoint.
Now the variables are:
usb_status = 1
Appli_state = APPLICATION_READY
fresult = FR_OK
Are we on the right track?
2024-01-17 3:05 PM
One more thing - The VBUS LED is on which I believe indicates that the USB voltage is on and within limits.
2024-01-17 3:08 PM - edited 2024-01-17 3:11 PM
Yep. usb_status = 1 -> mount = ok.
Should do...what you want , now. But first try to read only, check filename is correct ...
and breakpoints can be at mount or read from beginning on, just let it run , until there, thats all.
+ i am on track to my bed now. :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.