STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F429AGH6, delete a loaded program

I am working with the STM32F429AGH6 card, at first I had some problems to flash it, I managed to solve it using the boot mode 'hot plug' and I loaded a program that was sure to work and everything was perfect, then I tried to load a modified program ...

CarlosG by Associate
  • 1768 Views
  • 2 replies
  • 1 kudos

is CAN TERM pin high by default in B-G431B-ESC1?

Hi, I'm doing a project which sends CAN data from B-G431B-ESC1 board to sth else(NI cRio).Just to make sure, do I have to set CAN TERM Pin(PC14) high by setting it     GPIO_OUTPUT    GPIO output level : High or is it high by default?I don't understan...

JKong.3 by Associate III
  • 1252 Views
  • 0 replies
  • 0 kudos

Should be avoided using p->payload in LwIP examples?

I was looking at example HTTP IAP server provided in STM32F2xx package.\STM32Cube\Repository\STM32Cube_FW_F2_V1.9.3\Projects\STM322xG_EVAL\Applications\LwIP\LwIP_IAP\Src\httpserver.cIn http_recv, received data is extracted on every chunk of data from...

JMarq.1 by Associate III
  • 1859 Views
  • 2 replies
  • 0 kudos

Query on Class B library - STM32U585 MCU

Hi team; We have selected Trust zone MCU STM32U585ZIT6Q (U5 series) for our project.We are using with Trust zone enable in our project.we have a query regarding the X-CUBE-CLASSB-U5.We have taken library of X-CUBE-CLASSB-U5 and test example code in S...

JShah.7 by Associate III
  • 1628 Views
  • 1 replies
  • 0 kudos

HAL (Hard Animal Layer)

I thought I was the only one wondering how to implement DMA, but it seems to be different. I found this post, and found it interesting how the topic was addressed:To be honest, this was not a post I was planning on at first. However, I was working on...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.