2021-03-03 6:53 AM - last edited on 2025-05-01 2:57 AM by Andrew Neil
Is there a FreeRTOS demo program, using STM32CubeMX to set up, for:
STM3240G-EVAL - EVAL with STM32F407IG MCU or
STM32L476G-EVAL with STM32L476ZGT6 or
STM32F429IDISCOVERY with STM32F429ZIT6
Any help appreciated
I want to use STM32CubeMX to set upany of these eval boards, with FreeRTOS enabled, to create FreeRTOS code for testig
Solved! Go to Solution.
2021-03-03 7:33 AM
Hello @gerhard ,
There is no .ioc working project for FreeRTOS.
There is a rich set of FreeRTOS applications useful for your case with STM32cube packages that use HAL library and configured for different toolchains: EWARM, MDK-ARM, SW4STM32.
Try to pick the one suitable for the device and board you are using and start from it:
To start with STM32CubeMx, I advise you to refer to the "FreeRTOS" section in the UM1718 STM32CubeMx user Manual.
Have a look also to the UM1722 User manual about "Developing Applications on STM32Cube with RTOS", this will help you on FreeRTOS configuration.
Please mark my answer as the best by clicking the "Select as best" button if it helped you. This will help other users find this solution more quickly.
Imen
2021-03-03 7:33 AM
Hello @gerhard ,
There is no .ioc working project for FreeRTOS.
There is a rich set of FreeRTOS applications useful for your case with STM32cube packages that use HAL library and configured for different toolchains: EWARM, MDK-ARM, SW4STM32.
Try to pick the one suitable for the device and board you are using and start from it:
To start with STM32CubeMx, I advise you to refer to the "FreeRTOS" section in the UM1718 STM32CubeMx user Manual.
Have a look also to the UM1722 User manual about "Developing Applications on STM32Cube with RTOS", this will help you on FreeRTOS configuration.
Please mark my answer as the best by clicking the "Select as best" button if it helped you. This will help other users find this solution more quickly.
Imen
2021-03-04 7:36 AM
Thanks,
Very helpful information.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.