STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is there an example of reading and using audio from the on-board microphone of the STM32F469I Discovery kit? Details below

I am trying to access and read audio from the on-board microphone of my board and run it through a speech recognition model (Tensorflow lite speech commands). I am unable to find the audio library for my board or an example of accessing and using aud...

TSidd.3 by Associate II
  • 3388 Views
  • 5 replies
  • 0 kudos

hid usb device function

I'm using 'STM32F103RCT' and been create a HID Custom keyboard.When the HID Keyboard disconnects from the computer, is there a function that occurs?

JMOON.1 by Associate II
  • 760 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H7 Ethernet Not Working

Hi There,I am trying to run the ethernet example from the 1.7.0 version of the STM32H7 firmware at STM32Cube_FW_H7_V1.7.0\Projects\NUCLEO-H743ZI\Applications\LwIP\LwIP_HTTP_Server_Netconn_RTOS.The only modifications I have performed from the provided...

PMart.1 by Associate III
  • 13373 Views
  • 29 replies
  • 1 kudos

I ported an application from STM32L496RG to L4Q5. Most of application is working except the ADC acquisition because of DMA and the new DMAMUX1. I used the LL ST library unfortunately I didn't find any LL example of ADC + DMAMUX. Could you give examples?

ADC in dual mode with sampling frequency of 10.66 MS/s (5.33 per ADC).The System clock is set to 120 MHzThe ADC clock is set to 80MHzThe ADC1 IN8 ext3 is trigged by TIM2 CC2.The ADC data transfet is done though DMA2 CH3

Resolved! STM32G431 UCPD continuous power cycling

Hi,I'm developing an USB-C sink, using dead battery feature.I have respective CCx pins connected to DBCCx pins and the source can successfully power the sink.However, when the UCPD code starts running, the source disconects the 5V, effectively result...

STM32F769i-DISCO Ethernet Speed

Hello,I am using STM32F769i-DISCO board in my project. The project include camera module and I get data from this module using DCMI. I want to send this data to computer via ethernet. For this I need at least 100Mbits/s ethernet speed. But I cant f...

Baris by Associate
  • 748 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.