2020-07-10 11:38 AM
Hello,
In the application note AN2606, it is mentioned that ST's bootloader for STM32F446RE requires HSE clock if CAN bus is used to upload the hex file.
Now, if I am writing my own custom bootloader to upload the code via CAN, would I still need the HSE clock. Is possible to route HSI clock for the system clock and APB1
Thank you.
Snippet from AN2606
2020-07-10 12:44 PM
You can choose to clock it via any source you want, even ones which are out-of-spec. As long as you're willing to deal with things not work on an occasional unit, and support of that, you can use the HSI
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.