2018-08-12 10:24 AM
Hi all,
I am new to USB communication so please forgive my imprecisions.
I am using the discovery board STM32F469I-DISCO. I have been able to establish serial communication through the programming port (the port connected to the ST-link/V2-1) using usart3 as it is its default configuration. I would like to do the same using the USB OTG FS integrated. Is it possible? If so, how can I achieve it? In other words how do I make the board show up as a virtual com port and communicate through USART using the USB OTG FS port?
Thank you,
Frank
Solved! Go to Solution.
2018-08-12 11:19 AM
Well it's not going to manifest as a "USART" at the F4 end, but rather data through end-points
An example that might port over relatively easily
STM32Cube_FW_F4_V1.21.0\Projects\STM32469I_EVAL\Applications\USB_Device\CDC_Standalone
Or you could try your luck with CubeMX
2018-08-12 11:19 AM
Well it's not going to manifest as a "USART" at the F4 end, but rather data through end-points
An example that might port over relatively easily
STM32Cube_FW_F4_V1.21.0\Projects\STM32469I_EVAL\Applications\USB_Device\CDC_Standalone
Or you could try your luck with CubeMX
2018-08-12 1:25 PM
Very easy with the cube.
Select your device or board in the cube, select USB set it to CDC.
then follow the example, it works !
2018-08-12 1:44 PM
Actually, I use a true serial port for my work because when you use CDC , as your processor is reset, the CDC drops out and Windows has to adjust itself. then when your processor comes out of reset, the USB link is re-initialized and mostly works, but sometimes windows gets an error and doesn't recognize as a CDC port. then you need to "reset again and hold" until the device manager agrees it is a CDC port.
painful, so I use a MAX232 chip on my boards through a USB Dongle serial port which always remains connected in windows.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.