2022-08-16 5:53 PM
I already define the nucleo-STM32L476 as a USB microphone, but I want to know if it is possible to communicate with the microcontroller trough serial communication. I want to implement these feature because I want to change the digital filters that I am applying to the signal. For example, If I send the command ¨voice¨ trough serial, the microcontroller will select the filters that prioritize the voice and if then I send the command ¨guitar¨ I will be able to change the filters. I will appreciate any advice or help.
2022-08-17 3:14 PM
Do you want to add serial comms as an additional USB device (i.e. virtual COM port aka CDC)? Then, yes, but not necessarily straight forward. Search for "usb composite device". Some newer versions of the CubeMX/HAL libraries may have examples of composite device implementation. or look for the "tinyusb" project. [EDIT: presuming the L746 has enough endpoints - I didn't check]
Or do you want to serial comms via a UART. That is trivial (compared to USB).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.