2020-09-01 2:56 AM
I am using STM32F407 Controller For Ethernet Application , then Marvell 88E1116R PHY Chip i want to use with STM32F407 , so is it Compatible ?
2020-09-01 6:30 AM
STM32 doesn't support gigabit ethernet.
2020-09-01 9:13 PM
Thank you for your Answer, can i use 100MBPs or 10 MPBs with this Marvell 88E111R Phy Chip, My doubt is STM32F407 supporting MII/RMII and Marvell 88E1116R PHY Chip supporting GMII/GRMII so can i Interface??
if not possible which Phy IC i should use ??
thank you..
2020-09-02 7:13 AM
> Thank you for your Answer, can i use 100MBPs or 10 MPBs with this Marvell 88E111R Phy Chip, My doubt is STM32F407 supporting MII/RMII and Marvell 88E1116R PHY Chip supporting GMII/GRMII so can i Interface??
I don't know enough to know if GMII is backwards compatible with MII. Maybe it's like USB3 and you just have to wire it correctly. Not sure.
> if not possible which Phy IC i should use ??
Any PHY that supports MII or RMII should work. You could use one used on an ST board if you wanted.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.