2020-01-15 7:39 AM
Hello
I am struggling on how to init the USB device so that it recognized as a USB Audio device .
How do I transmit data.
How do I link the structures for device class properties
If I use CUBE Mx the generated code only gives an init.
The Audio Device class exmple is on STM32l476RG here it is implemented under the macro .
USB_OTG_MODE_DEVICE
stm32l452 generates under macro USB.
I need some guidance please help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.