2017-11-23 11:59 PM
Hi everyone!
I am using the I2C to write some data to two slave devices
this two devices need to drived by these imformation
The Board is STM32F429 discovery
the function I choose:
HAL_StatusTypeDef HAL_I2C_Mem_Write(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint16_t MemAddress, uint16_t MemAddSize, uint8_t *pData, uint16_t Size, uint32_t Timeout)
the full code is in the ZIP file
I'm not sure this function can be use in these project,have anybody could give me some advice?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.