2020-04-28 12:44 PM
2020-04-28 1:37 PM
'G0 with USB is said to be coming...
https://community.st.com/s/question/0D50X0000A4nkLBSQY/stm32g0x1-usb
JW
2020-04-28 1:13 PM
Simplest way is a USB serial adapter cable. Mind the voltage.
Most flexible is a Raspberry Pi, it can
2020-04-28 1:22 PM
Does anybody know why ST supported USB in some F0 MCUs but canceled to do it with G0 series MCUs? I was sure that G0 is the next generation of F0 and much better in all aspects.
2020-04-28 1:23 PM
Thanks fo your answer.
But what do you mean when you write that I can use USB with Zero and Zero W only. Can you please give some details?
2020-04-28 1:31 PM
The Zero models have a USB C-type port which can act both as a USB host or a USB device (gadget in Linux literature) just like a smartphone.
The normal size raspberries have USB A ports only, can't talk to a PC directly, because it too has USB A type ports.
2020-04-28 1:37 PM
'G0 with USB is said to be coming...
https://community.st.com/s/question/0D50X0000A4nkLBSQY/stm32g0x1-usb
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.