2021-09-12 2:41 AM
2021-09-12 7:06 AM
This question is lacking relevant details. Edit your post and add relevant information in the Details section.
2021-09-12 7:13 AM
thank you
i just need to know if it's possible to get data from pc to stm32f439zi USING USB not UART
2021-09-12 7:21 AM
2021-09-12 8:59 AM
Why would you even need to confirm this, don't the specification say it supports USB?
Writing application code might be more challenging.
YES, As USB VCP or MSC Device would have examples
STM32Cube_FW_F4_V1.24.0\Projects\STM324x9I_EVAL\Applications\USB_Device\CDC_Standalone
STM32Cube_FW_F4_V1.24.0\Projects\STM324x9I_EVAL\Applications\USB_Device\MSC_Standalone
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.