2022-04-30 11:56 AM
2022-04-30 12:26 PM
Have you seen this example?
Projects/STM32H735G-DK/Examples/ADC/ADC_DMA_Transfer
It assumes CN1 connected to PC2_C which is not the default on this board.
Need to solder SB41, SB42. See the User Manual for the board.
2022-06-13 4:25 PM
Looking at my board, it came with SB4 as OFF and SB5 as ON as expected from the user manual. However, SB41 and SB42 are both ON by default with 0 Ohm resistors. The manual suggests one should be OFF and on should be ON by default. Is the board wrong or the manual wrong?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.