2019-03-12 7:37 AM
I see in AN2606 in the section for the L4XXX and DFU bootloader the use of PA11 and PA12, but I don't know what I'm supposed to do with these to achieve DFU mode. I have created a port of micropython that has a firmware.dfu file for loading; however, it also has a firmware.bin, firmware.elf. Should I use the .dfu; or should I just use ST-LINK and load the .bin file? What if anything do I gain from using DFU bootloader mode?
2019-03-12 8:20 AM
Look for the BOOT0 pin, then install or uninstall the jumper/solder bridge as needed (check the data sheet and/or reference manual).
2019-03-12 12:40 PM
Not too keen about removing solder bridges. There is no removable jumper. So, I guess I'll just use st-link to load the .bin and leave the solder bridge as is.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.