STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPUART LL example - Rx not working

Hy everybody,I have a Nucleo 144-L496ZG board and I test the STM32Cube_FW_L4_V1.13.0 Examples_LL\LPUART\LPUART_WakeupFromStop2 example with IAR. The Tx is working (I see it on the PC's Realterm /TeraTerm) but the Rx doesn't. Even if I do not enter th...

sle by Associate
  • 1457 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to append data to a file in SD Card.

Hello,I am using a F413ZHTx Controller on a custom board. I am logging data onto the SD card using SDIO interface. Since I am logging a lot of data, I created a code to:1) Open the file on the SD card2) Log 100 entries3) Close the SD card file4) Reop...

STM with Fiber optic PHY.

Hi all, I'm looking for an STM microcontroller based eval-board/reference design, using only one Optical Phy. I would also like to have schematic and firmware support [preferred SPL] for the above requirements.Thanking with regardsAatif S...

STM32L073 - Jump to Bootaloader from user code

Hi,we are developing an application on a STM32L073RZT, that needs to jump to the embedded bootloader frim software, since we can not use the BOOT0 pin.I tried to write a code that jumps to system flash, using the NUCLEO-L073RZ board. In order to achi...

BSchm.7 by Associate
  • 913 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.