2025-01-21 5:03 AM
Hello!
I need to implement a task in FreeRTOS for my project that makes GET, POST, and PATCH requests to a server. So far, I have managed to send a UDP message to a specific port on a PC thanks to the following post:
Now, I would like to implement the task to send the requests. I have searched the forum but haven't found a clear conclusion. What catches my attention is that in the project I created with STM32CubeMX, there is the file http_client.h in Middleware -> Third_Party -> LwIP -> src -> include -> apps, but I can't find the http_client.c file with the functions.
I have found in the following link (https://github.com/yarrick/lwip/blob/master/src/apps/http/http_client.c) I have copy the http folder in Middleware -> Third_Party -> LwIP -> src -> apps.
And I have tried with the following code:
void http_get_task(void const *pvParameters) {
// Initialize the LWIP stack (only if not already initialized elsewhere)
lwip_init();
// HTTP connection settings
httpc_connection_t settings;
settings.use_proxy = 0; // No proxy
settings.result_fn = http_result_callback;
settings.headers_done_fn = http_headers_done_callback;
ip_addr_t server_addr;
IP4_ADDR(&server_addr, 192, 168, 4, 250); // Server IP address
const char *uri = "/path/to/resource"; // Resource URI
u16_t port = 3000; // Server port
httpc_state_t *connection = NULL;
// Make the HTTP GET request
err_t err = httpc_get_file(&server_addr, port, uri, &settings, NULL, NULL, &connection);
if (err != ERR_OK) {
printf("Failed to start HTTP GET request. Error: %d\n", err);
vTaskDelete(NULL); // Delete the task if the request fails
return;
}
printf("HTTP GET request initiated. Waiting for response...\n");
// Main task loop to handle timeouts and connection
while (connection != NULL) {
sys_check_timeouts(); // Process LWIP timeouts
vTaskDelay(pdMS_TO_TICKS(100)); // Delay to avoid busy-waiting
}
printf("Task complete. Exiting.\n");
vTaskDelete(NULL); // Delete the task when done
}
When compilig the next error appears: undefined reference to `httpc_get_file' main.c. I have included the http_client.h in main.c (#include "lwip/apps/http_client.h"). Also I have verified that the macros LWIP_TCP && LWIP_CALLBACK_API are at 1.
Apart from these compilation issues, I wonder if I am heading in the right direction or if there is another way to set up an HTTP client. Any help is welcome, thanks. :)
Solved! Go to Solution.
2025-01-28 12:18 AM - edited 2025-01-28 12:19 AM
Hello!
Nom I am able to make a PATCH request to my server. I have tested since the weekend. 2.000.000 PATCH request done without any error.
I attach the modified http_client.c file. I have created the httpc_patch_file function in orther to allow to send a token in the header and a json body.
I hope this helps somebody
2025-01-21 5:19 AM
@RafaelS wrote:When compiling the next error appears: undefined reference to `httpc_get_file' main.c.
It's telling you that it can't find any definition for the httpc_get_file() function.
@RafaelS wrote:I have included the http_client.h in main.c (#include "lwip/apps/http_client.h")
A header file would not be expected to provide a definition - just a declaration (aka "prototype").
So do you actually have a .c file in your project which does define the httpc_get_file() function?
2025-01-21 5:32 AM
Hello Andrew,
I have download the http folder from https://github.com/yarrick/lwip/tree/master/src/apps/http,
and after I have added the path of the folder in the Include paths of MCU/MPU GCC Compiler.
In the http folder there is an http_client.c that define the httpc_get_file https://github.com/yarrick/lwip/blob/master/src/apps/http/http_client.c in line 641.
2025-01-21 5:35 AM
Well, your linker is not seeing that.
Is that file actually getting built?
2025-01-21 8:25 AM
I have selected the option -v and yes, the file are not getting built. I have copied the folder http outside of CM7 project.
I have moved the folder in CM7 and now the function httpc_get_file is compiled.
There were another compiling errors due to some file in makefsdata folder is for WIN or LINUX. In makefsdata.c ->
#ifdef WIN32
#define GETCWD(path, len) GetCurrentDirectoryA(len, path)
#define GETCWD_SUCCEEDED(ret) (ret != 0)
#define CHDIR(path) SetCurrentDirectoryA(path)
#define CHDIR_SUCCEEDED(ret) (ret == TRUE)
#elif __linux__ || __APPLE__
#define GETCWD(path, len) getcwd(path, len)
#define GETCWD_SUCCEEDED(ret) (ret != NULL)
#define CHDIR(path) chdir(path)
#define CHDIR_SUCCEEDED(ret) (ret == 0)
#else
#error makefsdata not supported on this platform
#endif
I have deleted the files related to fs, and now there are no compilation errors... but I am not confident that the library I downloaded is suitable for a microcontroller.
Anyway, I have programmed the STM32H745, and the debugger in httpc_get_file function returns an "invalid parameters" error. I will review the function's consistency and the parameters supplied.
2025-01-28 12:18 AM - edited 2025-01-28 12:19 AM
Hello!
Nom I am able to make a PATCH request to my server. I have tested since the weekend. 2.000.000 PATCH request done without any error.
I attach the modified http_client.c file. I have created the httpc_patch_file function in orther to allow to send a token in the header and a json body.
I hope this helps somebody
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.