2025-04-10 6:57 AM
hi all,
I am using STM32F733xx and i want to read the Vout i will be monitoring is between 1-5v, to read that i have used analogue pins PG13, PH3 ,PH2,PG14, PE2,PE3, PE6, PE4,PE5,PF1,PF0,PF2
I already have the PCB so i cant change the design can anyone suggest any solution to this?
Looking for some firmware based solution to this problem.
Thanks in advance,
Regards,
Sal
Solved! Go to Solution.
2025-04-16 10:53 PM
Thanks everyone i ended up changing the pin outs and modified the hardware.
Also for the voltage level my input is up to 5v which IC i should use in between in order to change the voltage level but to get the accurate voltage and current reading?
2025-04-10 7:19 AM
Welcome to the forum.
For best results, please see: How to write your question to maximize your chances to find a solution.
@sal92 wrote:i have used analogue pins PG13, PH3 ,PH2,PG14, PE2,PE3, PE6, PE4,PE5,PF1,PF0,PF2
None of those pins has any analogue function:
PG13 TRACED0, LPTIM1_OUT,USART6_CTS, FMC_A24,EVENTOUT
PH3 QUADSPI_BK2_IO1,SAI2_MCK_B, FMC_SDNE0,EVENTOUT
PH2 LPTIM1_IN2, QUADSPI_BK2_IO0, SAI2_SCK_B, FMC_SDCKE0, EVENTOUT
PG14 TRACED1, LPTIM1_ETR,USART6_TX,QUADSPI_BK2_IO3, FMC_A25,EVENTOUT
PE2 TRACECLK, SPI4_SCK, SAI1_MCLK_A, QUADSPI_BK1_IO2, FMC_A23, EVENTOUT
PE3 TRACED0, SAI1_SD_B, FMC_A19, EVENTOUT
PE6 TRACED3, TIM1_BKIN2,TIM9_CH2, SPI4_MOSI,SAI1_SD_A, SAI2_MCK_B,FMC_A22, EVENTOUT
PE4 TRACED1, SPI4_NSS,SAI1_FS_A, FMC_A20,EVENTOUT
PE5 TRACED2, TIM9_CH1,SPI4_MISO, SAI1_SCK_A,FMC_A21, EVENTOUT
PF1 I2C2_SCL, FMC_A1, EVENTOUT
PF0 I2C2_SDA, FMC_A0, EVENTOUT
PF2 I2C2_SMBA, FMC_A2, EVENTOUT
Please show your schematic - that would be easier to follow.
An ADC is the only way you're going to directly read an analogue voltage as a digital value.
Otherwise, you're going to have to "synthesise" an ADC; eg, use a DAC to generate a "reference", and a comparator to compare.
Whatever you do, it's going to need hardware changes...
2025-04-10 5:57 PM
Even if they were wired to the correct pins, the ADC isn't going to be able to measure 5 V.
2025-04-16 12:14 PM
Hi @sal92
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
2025-04-16 10:53 PM
Thanks everyone i ended up changing the pin outs and modified the hardware.
Also for the voltage level my input is up to 5v which IC i should use in between in order to change the voltage level but to get the accurate voltage and current reading?
2025-04-17 1:17 AM
@sal92 wrote:Thanks everyone i ended up changing the pin outs and modified the hardware.
That's good - please mark the solution:
https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256
@sal92 wrote:Also for the voltage level my input is up to 5v which IC i should use in between in order to change the voltage level but to get the accurate voltage and current reading?
That's a separate question - please start a new thread for that.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.