2020-03-16 12:24 AM
Platform: Nucleo L432KC
Sw: FreeRTOS generated by STM32CubeIDE
Description:
The maximum level of `configMAX_SYSCALL_INTERRUPT_PRIORITY` is 1 with declaration in FreeRTOSConfig.h as below.
#define configMAX_SYSCALL_INTERRUPT_PRIORITY ( configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY << (8 - configPRIO_BITS) )However, the minimum Preemption Priority level of any interrupt source e.g. and edge interrupt is 15. That means it is above the max. level of `configMAX_SYSCALL_INTERRUPT_PRIORITY`.
How to set correct priority levels if I want to call an ISR-safe function from edge interrupt?
2020-03-16 12:41 AM
https://lmgtfy.com/?q=configMAX_SYSCALL_INTERRUPT_PRIORITY
For STM32 the value of 16 is a complete nonsense...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.