2018-06-05 1:30 PM
Hello guys.
When I used LPC17xx series in my last experience of ARM MCUs I used 2 timers one for generating interrupt every 1 second and one for counting the rising edges of the input CAP.
So I started reading the Reference menu of the stm32F2xx ,but there were a lot of timer functions described in timer section.I was confused which one to use for my purpose.
Now I know that how to set the timer to work as a TIME BASE,but for input I didn't know which one to use.One section described external clock mode 1 and the other external clock mode 2 and the other was input capture mode .
Which one should I use?
#stm32f2 #cube-hal2018-06-07 5:22 PM
'
Which one should I use?'
it depends on what you are trying to do.
The basic form of measuring frequency is to compare / gate two pulse trains, one of unknown frequency, and another of known frequency.
1) the typical way is to use the known pulse train to generate a time base that turns on / off the counting of the unknown pulse train; this works for high frequency signal;
2) it can also be done the other way around: using the unknown pulse train to gate the known pulse train -> aka a reciprocal counter; it works for lower frequency measurement.
3) for cases where you don't need super high precision and the input pulse train isn't too fast / slow, you can use input capture to measure the frequency as well.
there are other ways too. all depends on what kind of signal you are trying to measure.
2018-06-07 6:33 PM
Sorry don't use CubeMX
The PWMInput examples should use CH1 and CH2 to report period and duty, and reset
STM32Cube_FW_F4_V1.21.0\Projects\STM32F4-Discovery\Examples\TIM\TIM_PWMInput\Src\main.c
/*♯♯-1- Configure the TIM peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
/* Set TIMx instance */ TimHandle.Instance = TIM2;/* Initialize TIMx peripheral as follow:
+ Period = 0xFFFFFFFF + Prescaler = 0 + ClockDivision = 0 + Counter direction = Up */ TimHandle.Init.Period = 0xFFFFFFFF; TimHandle.Init.Prescaler = 0; TimHandle.Init.ClockDivision = 0; TimHandle.Init.CounterMode = TIM_COUNTERMODE_UP; if(HAL_TIM_IC_Init(&TimHandle) != HAL_OK) { /* Initialization Error */ Error_Handler(); }/*♯♯-2- Configure the Input Capture channels ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
/* Common configuration */ sConfig.ICPrescaler = TIM_ICPSC_DIV1; sConfig.ICFilter = 0;/* Configure the Input Capture of channel 1 */
sConfig.ICPolarity = TIM_ICPOLARITY_FALLING; sConfig.ICSelection = TIM_ICSELECTION_INDIRECTTI; if(HAL_TIM_IC_ConfigChannel(&TimHandle, &sConfig, TIM_CHANNEL_1) != HAL_OK) { /* Configuration Error */ Error_Handler(); }/* Configure the Input Capture of channel 2 */
sConfig.ICPolarity = TIM_ICPOLARITY_RISING; sConfig.ICSelection = TIM_ICSELECTION_DIRECTTI; if(HAL_TIM_IC_ConfigChannel(&TimHandle, &sConfig, TIM_CHANNEL_2) != HAL_OK) { /* Configuration Error */ Error_Handler(); } /*♯♯-3- Configure the slave mode ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ /* Select the slave Mode: Reset Mode */ sSlaveConfig.SlaveMode = TIM_SLAVEMODE_RESET; sSlaveConfig.InputTrigger = TIM_TS_TI2FP2; if(HAL_TIM_SlaveConfigSynchronization(&TimHandle, &sSlaveConfig) != HAL_OK) { /* Configuration Error */ Error_Handler(); }/*♯♯-4- Start the Input Capture in interrupt mode ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
if(HAL_TIM_IC_Start_IT(&TimHandle, TIM_CHANNEL_2) != HAL_OK) { /* Starting Error */ Error_Handler(); }/*♯♯-5- Start the Input Capture in interrupt mode ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
if(HAL_TIM_IC_Start_IT(&TimHandle, TIM_CHANNEL_1) != HAL_OK) { /* Starting Error */ Error_Handler(); }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.