2022-04-05 4:07 AM
Hello everyone,
I want to make an USB microphone using the STM32CubeIDE. After I configured the USB connection with STM32CubeMX, I wanted to modify the USB device library to make it work in the other direction (from device to host). Therefore I modified the descriptors and the functions USBD_AUDIO_Init and USBD_AUDIO_DataIn.
When I plug the MCU into my PC, it is correctly recognized as USB microphone, so the descriptors are alright I guess. But it is not possible to record the generated audio samples from the MCU with e.g. Audacity.
So the basic problem is the isochronous data transfer. Then I recorded the USB connection with Wireshark and I figured out that the MCU answers the requests from the host but there are no audio data in the response. I tried to debug the code and I also figured out that the USBD_AUDIO_DataIn function is not called, so the endpoint number seems to be always 0.
So basically I have two questions:
Why is the endpoint number always 0 and the USBD_AUDIO_DataIn are not called?
What is necessary to let the USB device library work in the other direction (as microphone)?
Thank you for helping.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.