STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have an STM32H742VGT based project with ethernet connection (LAN8742AI-CZ phy ) the problem is that I get HAL_ERROR when the HAL_StatusTypeDef HAL_ETH_Transmit(ETH_HandleTypeDef *heth, ETH_TxPacketConfig *pTxConfig, uint32_t Timeout)

When the HAL_ETH_Transmit is called by the driver it seems the code below (part of HAL_ETH_Transmit ) times out as the DMA TX complete callback are not called. I've followed the STM32H743 example but I guess STM32H742 memory map is a bit different th...

NMach.1 by Associate II
  • 5025 Views
  • 9 replies
  • 0 kudos

TIMER and GPIO PIN

Hello,I'm have a Nucleo board with a STM32F334R8T6I configured a timer with 10kHz and I'm using the HAL_TIM_PeriodElapsedCallback to call a funtion that will control my motor and read some data with the ADC. I want to check the frequency that the con...

Nakata_2-1722018201849.png Nakata_0-1722018043049.png Nakata_1-1722018123342.png
Nakata by Associate II
  • 1391 Views
  • 2 replies
  • 1 kudos

Resolved! STM32F407 USB bootloader problem

Hi,Recently I had to replace the MCU in a device and I tried to upload the code using USB Bootloader, as it is available and requires very little stuff when you're on site.So, the MCU has been detected in the system (see PIC1.png), but the CubeProgra...

Resolved! ThreadX does not start scheduling

Hi,my application is loaded via the bootloader and i sstarted. Two threads are generated and it seems properly generated because one thread is in ready state while the other is in suspended state.Systick is used for the ThreadX and TIM6 is used for t...

SHaue.2 by Associate II
  • 3824 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.