2025-11-26 12:49 AM - last edited on 2025-12-01 7:38 AM by mƎALLEm
Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code.
Hi All,
MCU is STM32H563. I attempted to jump from the Secure App directly to the System Bootloader so that I could program the OBK file without pulling BOOT0 high.
However, using the method below, the jump never succeeds — the MCU keeps resetting continuously.
Sometimes it resets immediately, and sometimes it reaches the reset vector of the system bootloader and then resets again.
static void JumpToBootloader(void)
{
funcptr_NS NonSecure_ResetHandler;
__disable_irq(); // Disable interrupts
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
HAL_RCC_DeInit(); // Reset clock configuration
for (int i = 0; i < sizeof(NVIC->ICER) / sizeof(NVIC->ICER[0]); i++) {
NVIC->ICER[i] = 0xFFFFFFFF;
NVIC->ICPR[i] = 0xFFFFFFFF;
}
__DSB(); __ISB();
SCB_NS->VTOR = BOOTLOADER_BASE_NS;
/* Set non-secure main stack (MSP_NS) */
__TZ_set_MSP_NS((*(uint32_t *)BOOTLOADER_BASE_NS));
/* Get non-secure reset handler */
NonSecure_ResetHandler = (funcptr_NS)(*((uint32_t *)((BOOTLOADER_BASE_NS) + 4U)));
/* Start non-secure state software application */
NonSecure_ResetHandler();
}
From the documentation AN2606 (page 54), I learned that the System Bootloader version in the H563 is Boot_V3_2, which includes the following statement:
Before jumping to the BL, the SFSP maps all the resources needed by the BL
to the non-secure domain. A jump from the BL (“Go” command) to an
application using other resources does not work.
So does this mean that jumping directly to the BL address without going through SFSP cannot succeed?
2026-01-19 1:49 PM
Hello @deposition
As mentioned in AN2606, SFSP first runs and maps all required resources to the Non‑Secure domain.
A direct jump from your Secure application to the bootloader address bypasses SFSP, so the bootloader does not find the expected environment and this typically causes the resets you see.
To use the bootloader, you should:
With regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.