2024-03-11 4:50 PM
STM32CubeU5/Projects/B-U585I-IOT02A/Applications/FileX at main · STMicroelectronics/STM32CubeU5 (github.com).
Here the example is to create the STM.TXT in the run-time
/* Create a file called STM32.TXT in the root directory. */
nor_ospi_status = fx_file_create(&nor_ospi_flash_disk, "STM32.TXT");
But I have my pre-configured config.ini file and cacert.pem files and want flash them in stm32
How can inject them into the stm32 target? Could you please share an example of it?
2024-03-11 5:06 PM
Make as an array of bytes, perhaps use your C skills to use STDIO file functions to read and process on your host PC.
Different tools have things like INCBIN to pull in files to the Linker or assembler.
2024-03-11 5:35 PM - edited 2024-03-11 5:36 PM
thanks for the info
Could you please give me some references
is there any alternative ways to achieve it
in my case I will use ini parser to read the all configuration values from ini file
and I will update the specific configuration value at runtime based on the requirement
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.