2019-12-10 4:51 AM
I have a STM32F103C8T card, I am developing an application that receives a byte array by usb / serial.
I have a variable "uint8_t USBBuffer;" in "usbd_cdc_if.c" which stores the bytes.
My question is: how can a non-vector variable receive an external multi-byte vector?
One of the vectors I get is this: {0x16, 0x16, 0x02, 0x00, 0x10, 0x03, 0x00, 0x00, 0x03}
I realized that I can store these bytes in a single index of a vector, eg: USBBuffer2 [0] = USBBuffer;
With this I can easily transmit USBBuffer2 with the CDC_Transmit function.
My question is, how is this vector stored in a uint8_t that is not a vector? how can i compare with another uint8_t variable?
Thanks in advance.
And I'm sorry if noob's question is that I'm just starting out in this universe.
2019-12-10 5:55 AM
Perhaps review chapter on pointers in C?
&USBBuffer would be the address for a uint8_t one byte array
You can use memcmp() to compare one or multiple bytes in memory.
Or do
if (a == x[i]) puts("same");
2019-12-10 6:24 AM
I have tried memcmp and have not been successful.
I've tried comparing with "if (var1 [i] == USBBuffer [i])" but as I mentioned earlier all bytes are in USBBuffer [0] and var1 [] = {0x16, 0x16, 0x02, 0x00, 0x10, 0x03 , 0x00, 0x00, 0x03}.
The problem is, I can't print USBBuffer to know how bytes are saved.
This would be easily solved if I have been using the Arduino IDE, but unfortunately my external application does not recognize my STM32 card if it is not recorded with STM32cubeIDE, I still can't figure out why.
2019-12-10 6:58 AM
>>I have tried memcmp and have not been successful.
Probably because you're trying to compare one thing against a dozen things.
uint8_t USBBuffer = 0x12;
printf("%02X\n", USBBuffer);
Or make a memory dumping function
dumpdata(16, &USBBuffer); // The byte that USBBuffer holds, and those surrounding it
>>I've tried comparing with "if (var1 [i] == USBBuffer [i])" but as I mentioned earlier all bytes are in USBBuffer [0] and var1 [] = {0x16, 0x16, 0x02, 0x00, 0x10, 0x03 , 0x00, 0x00, 0x03}.
Ok, but there's only ONE byte in your application of USBBuffer, you're going to have to accumulate bytes if you want to compare against multiples.
// Does byte match vector/array index i
if (var1 [i] == USBBuffer) printf("Byte Level match at %d\n", i);
// Accumulate a byte into an array
uint8_t BiggerBuffer[100], *p = BiggerBuffer;
...
*p++ = USBBuffer; // For each received byte to fill array
Trick here is
a) Understand data representation in memory properly
b) Learn C, variables, arrays
c) Learn Pointers
2019-12-10 7:03 AM
I really have a lot to learn yet, probably USBBuffer is just a pointer, I will deepen my studies in C.
Thank you very much.
2019-12-18 1:43 PM
Dear friend, thank you so much for your help, I finally managed to make the code.
I was trying to compare a single byte with an entire vector, I had no idea how fast this chip was processing.
Thanks again.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.