STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401 USB remote wakeup does not work

Environment:STM32F401RCUSB HID device, Full speedfreeRTOSProblem:Device can send/receive data to/from host and can be put in suspend state and resume from suspend state.However, the remote wake-up function never worksCode:My USB remote wake up log in...

Resolved! STM32L475RG - Having trouble jumping between multiple .bin programs in flash, program stops working.

CURRENT PRODUCT Our existing devices have a custom USB DFU bootloader starting at address 0x08000000. Our main application starts at 0x08008000, after 32Kb of space. I can jump from the main app to the bootloader with no issues (using a NVIC_Systemre...

RSikk.493 by Associate II
  • 2003 Views
  • 5 replies
  • 0 kudos

Hi, We are looking for an IoT Gateway based on STM32 MCU's, the primary reason for going with MCU's is the Low Power consumption feature of these devices, can any suggest me the suitable board/dev kit for our purpose.

As STM32F4 series can run an RTOS,RTOS like FREE RTOS is optimal to use to run multiple threads for our need, can this combination of FREE RTOS and Low Power Gateway on STM32 can be achievable in ST platform, please guide.

Resolved! Can't meet STM32G0 power spec in "Low Power sleep" mode

I had using sample code "low power sleep mode", the current measure result is over datasheet spec, how to do can get datasheet value?The measurement result is around 1mA, the datasheet show 60uA.​Hardware paltform: NUCLEO-G071RBSoftware version: 1.3....

Felix1 by Associate II
  • 1308 Views
  • 2 replies
  • 0 kudos

USB and CAN not working at same time ?

Hi,I am using STM32F7 and I'm trying to make USB and CAN work.But i am finding issues in making it work at same time.I have generated the project via cubeMX .I have set the PLLM i.e.,Division factor for PLL VCO input clock as 8 and PLLN i.,eMultiplic...

VPras by Associate II
  • 878 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.