2022-03-08 3:49 AM
I'm working with the board B-4SI-IOTI and I'm trying to program the board with the Provisioning.bin file from package X-CUBE-AWS. The first time it works but now appears this message on the terminal:
-------------------------------------------------------------------------------
Start provisioning of STSAFE-A
Force STSAFE-A provisioning
Launching STSAFE-A pairing
Check if Pairing Host keys available
Please check User configuration, Option Byte DBANK must be DBANK=0
Pairing NOK, End of Provisioning
-------------------------------------------------------------------------------
I do not change the files from the package and now I don't know what I have to do to solve this, and I don't find previous questions with this problem.
Thanks for all and waiting for any help :)
2022-03-10 1:23 AM
Use STM32CubeProgrammer :
In the STM32CubeProgrammer GUI, connect to the B-L4S5I-IOT01A board. click on "OB" icon (option bytes). open "user configuration" section. scroll to DBANK setting. set it to what is required (single bank - unchecked - 0).
2022-03-10 4:22 AM
I change it, but then do not appear the message in terminal that has to be printed, only appears Start provisioning of STSAFE-A but do not give feedback about it the provisioning, erase data and store certificates are OK or NOK..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.