2021-02-26 12:42 AM
Is there a way to use the HAL library to read the variable specified in the address?
Solved! Go to Solution.
2021-03-08 1:42 AM
Hi @リョウスケ クボ ,
A ready to use example for NUCLEO-L073RZ is available under STM32Cube_FW_L0\Projects\NUCLEO-L073RZ\Examples_LL\ADC\ADC_TemperatureSensor\Src.
You can refer to the readme.txt file on the same folder that describes what is expected by the example and how to use it.
The calibration is one of the operations done when calling Activate_ADC thanks to the LL API LL_ADC_StartCalibration.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-03-08 1:42 AM
Hi @リョウスケ クボ ,
A ready to use example for NUCLEO-L073RZ is available under STM32Cube_FW_L0\Projects\NUCLEO-L073RZ\Examples_LL\ADC\ADC_TemperatureSensor\Src.
You can refer to the readme.txt file on the same folder that describes what is expected by the example and how to use it.
The calibration is one of the operations done when calling Activate_ADC thanks to the LL API LL_ADC_StartCalibration.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-03-10 12:21 AM
Hello Amel NASRI (ST Employee)
Thank you for answer my question.
I was able to solve it.
I confirmed that it can be configured with the function of
__LL_ADC_CALC_TEMPERATURE (VDDA_APPLI, uhADCxConvertedData, LL_ADC_RESOLUTION_12B);
regard.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.