2022-09-08 5:06 AM
/////////////////////////////////////////////////////
//Add 3 IAD class here // this one is for COM port 3
0x08, // bLength: Interface Descriptor size
0x0B, // bDescriptorType: IAD
0x04, // bFirstInterface
0x03, // bInterfaceCount
0x02, // bFunctionClass: CDC
0x02, // bFunctionSubClass
0x01, // bFunctionProtocol
0x02, // iFunction
/*Interface Descriptor */
0x09, /* bLength: Interface Descriptor size */
USB_DESC_TYPE_INTERFACE, /* bDescriptorType: Interface */
/* Interface descriptor type */
0x00+4, /* bInterfaceNumber: Number of Interface */
0x00, /* bAlternateSetting: Alternate setting */
0x01, /* bNumEndpoints: One endpoints used */
0x02, /* bInterfaceClass: Communication Interface Class */
0x02, /* bInterfaceSubClass: Abstract Control Model */
0x01, /* bInterfaceProtocol: Common AT commands */
0x00, /* iInterface: */
/*Header Functional Descriptor*/
0x05, /* bLength: Endpoint Descriptor size */
0x24, /* bDescriptorType: CS_INTERFACE */
0x00, /* bDescriptorSubtype: Header Func Desc */
0x10, /* bcdCDC: spec release number */
0x01,
/*Call Management Functional Descriptor*/
0x05, /* bFunctionLength */
0x24, /* bDescriptorType: CS_INTERFACE */
0x01, /* bDescriptorSubtype: Call Management Func Desc */
0x00, /* bmCapabilities: D0+D1 */
0x01 + 4 , /* bDataInterface: 1+2 */
/*ACM Functional Descriptor*/
0x04, /* bFunctionLength */
0x24, /* bDescriptorType: CS_INTERFACE */
0x02, /* bDescriptorSubtype: Abstract Control Management desc */
0x02, /* bmCapabilities */
/*Union Functional Descriptor*/
0x05, /* bFunctionLength */
0x24, /* bDescriptorType: CS_INTERFACE */
0x06, /* bDescriptorSubtype: Union func desc */
0x00+4, /* bMasterInterface: Communication class interface */
0x01+4, /* bSlaveInterface0: Data Class Interface */
/*Endpoint 2 Descriptor*/
0x07, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType: Endpoint */
CDC_CMD_EP+3, /* bEndpointAddress */
0x03, /* bmAttributes: Interrupt */
LOBYTE(CDC_CMD_PACKET_SIZE), /* wMaxPacketSize: */
HIBYTE(CDC_CMD_PACKET_SIZE),
0x10, /* bInterval: */
/*---------------------------------------------------------------------------*/
/*Data class interface descriptor*/
0x09, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_INTERFACE, /* bDescriptorType: */
0x01+4, /* bInterfaceNumber: Number of Interface */
0x00, /* bAlternateSetting: Alternate setting */
0x02, /* bNumEndpoints: Two endpoints used */
0x0A, /* bInterfaceClass: CDC */
0x00, /* bInterfaceSubClass: */
0x00, /* bInterfaceProtocol: */
0x00, /* iInterface: */
/*Endpoint OUT Descriptor*/
0x07, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType: Endpoint */
CDC_OUT_EP+4, /* bEndpointAddress */
0x02, /* bmAttributes: Bulk */
LOBYTE(CDC_DATA_FS_MAX_PACKET_SIZE), /* wMaxPacketSize: */
HIBYTE(CDC_DATA_FS_MAX_PACKET_SIZE),
0x00, /* bInterval: ignore for Bulk transfer */
/*Endpoint IN Descriptor*/
0x07, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType: Endpoint */
CDC_IN_EP+4, /* bEndpointAddress */
0x02, /* bmAttributes: Bulk */
LOBYTE(CDC_DATA_FS_MAX_PACKET_SIZE), /* wMaxPacketSize: */
HIBYTE(CDC_DATA_FS_MAX_PACKET_SIZE),
0x00 /* bInterval: ignore for Bulk transfer */
//EP+3---------------------------------------------------------->
/* Open EP IN */
(void)USBD_LL_OpenEP(pdev, CDC_IN_EP+4, USBD_EP_TYPE_BULK,
CDC_DATA_HS_IN_PACKET_SIZE);
pdev->ep_in[(CDC_IN_EP+4) & 0xFU].is_used = 1U;
/* Open EP OUT */
(void)USBD_LL_OpenEP(pdev, CDC_OUT_EP+4, USBD_EP_TYPE_BULK,
CDC_DATA_HS_OUT_PACKET_SIZE);
pdev->ep_out[(CDC_OUT_EP+4) & 0xFU].is_used = 1U;
/* Set bInterval for CDC CMD Endpoint */
pdev->ep_in[(CDC_CMD_EP+4) & 0xFU].bInterval = CDC_HS_BINTERVAL;
//EP+3---------------------------------------------------------------->
/* Open EP IN */
(void)USBD_LL_OpenEP(pdev, CDC_IN_EP+4, USBD_EP_TYPE_BULK,
CDC_DATA_FS_IN_PACKET_SIZE);
pdev->ep_in[(CDC_IN_EP+4) & 0xFU].is_used = 1U;
/* Open EP OUT */
(void)USBD_LL_OpenEP(pdev, CDC_OUT_EP+4, USBD_EP_TYPE_BULK,
CDC_DATA_FS_OUT_PACKET_SIZE);
pdev->ep_out[(CDC_OUT_EP+4) & 0xFU].is_used = 1U;
/* Set bInterval for CMD Endpoint */
pdev->ep_in[(CDC_CMD_EP+4) & 0xFU].bInterval = CDC_FS_BINTERVAL;
(void)USBD_LL_OpenEP(pdev, CDC_CMD_EP+4, USBD_EP_TYPE_INTR, CDC_CMD_PACKET_SIZE);
pdev->ep_in[(CDC_CMD_EP+4) & 0xFU].is_used = 1U;
/* Prepare Out endpoint to receive next packet */
USBD_LL_PrepareReceive(pdev,
CDC_OUT_EP+4,
hcdc->RxBuffer,
CDC_DATA_HS_OUT_PACKET_SIZE);
/* Prepare Out endpoint to receive next packet */
USBD_LL_PrepareReceive(pdev,
CDC_OUT_EP+4,
hcdc->RxBuffer,
CDC_DATA_FS_OUT_PACKET_SIZE);
//-------------------->EP+4
/* Close EP IN */
(void)USBD_LL_CloseEP(pdev, CDC_IN_EP+3);
pdev->ep_in[(CDC_IN_EP+4) & 0xFU].is_used = 0U;
/* Close EP OUT */
(void)USBD_LL_CloseEP(pdev, CDC_OUT_EP+3);
pdev->ep_out[(CDC_OUT_EP+4) & 0xFU].is_used = 0U;
/* Close Command IN EP */
(void)USBD_LL_CloseEP(pdev, CDC_CMD_EP+3);
pdev->ep_in[(CDC_CMD_EP+4) & 0xFU].is_used = 0U;
pdev->ep_in[(CDC_CMD_EP+4) & 0xFU].bInterval = 0U;
2022-09-08 9:23 AM
IAD bInterfaceCount you have 0x03, should be 0x02. You have 3 endpoints but only 2 interfaces per CDC/VCOM
Endpoint2 descriptor, EP address looks funny ("+3"), maybe that should be +4 like all your other EP increments?
2023-03-03 1:13 PM
You may need to update the FIFO settings for each additional endpoint you create.
2023-03-03 2:40 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.