STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32Cube FW_G4 V1.4.0 breaks USB HID communication

I have been having much difficulty trying to port a custom USB HID protocol from a previous project using the STM32F405 to the STM32G431. Connection would initially be established, immediately followed by pipe errors. Eventually I found that if I dow...

BPaik by Senior
  • 6859 Views
  • 12 replies
  • 0 kudos

HAL_LPTIM_Counter_Start_IT returning HAL_TIMEOUT

Hi. I am using STM32L412KBTx for my application. I am using LPTIM for 150ms and 5s timings.The pattern is like 150ms-->5s-->150ms whenever data is received over LPUART.So, for first 150ms timeout value, it runs fine and when I start for 5s timeout va...

0693W00000QNrgAQAT.png 0693W00000QNrgPQAT.png 0693W00000QNrgjQAD.png 0693W00000QNrhIQAT.png
SBhon.1 by Associate III
  • 3260 Views
  • 3 replies
  • 0 kudos

Resolved! - Main Config: These peripherals still have some not configured or wrong parameter values: [CORTEX M7] getting error

Hello ,I am working on NUCLEO-H745ziq board. I am trying the example AZURE RTOS of Ux_CDC_device , the example provide in cubemx accordingly I setup the things in cubemx but when I try to generate the code it shows warning and the when I run the pro...

0693W00000QKISWQA5.png
MDeva.1 by Associate II
  • 5572 Views
  • 1 replies
  • 0 kudos

Is it possible to incorporate serial communication to a STM32L476 that is already defined as a USB Audio device?

I already define the nucleo-STM32L476 as a USB microphone, but I want to know if it is possible to communicate with the microcontroller trough serial communication. I want to implement these feature because I want to change the digital filters that I...

JacquiG29 by Associate II
  • 1577 Views
  • 1 replies
  • 0 kudos

STM32H747 and USB DISK - how to make it work?

Discovery board: STM32H747I-DISCO.OTG connected to P1 (HS).First of all, there are two modes:EXTERNAL PhyInternal FSEXTERNAL Phy is faster, Internal FS is slower. What does "external" mean?Will it just work or not?First I tried "Internal FS". Just do...

HTD by Senior III
  • 3947 Views
  • 6 replies
  • 0 kudos

Resolved! Are there any guides on how to include X-CUBE-USB-AUDIO functionality into an STM32CubeIde project (.ioc)?

Hello, I am looking to include USB audio streaming, this package looks perfect for handling a lot of the functionality. Just wondering if there are any guides on how to add this to a .ioc STM32CubeIde project for a different part than those in the Ex...

WFunk.1 by Associate
  • 1928 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.