2022-08-17 7:15 PM
I made a High Speed USB DEVICE using USB PHY with STM32F207.
A data transmission test to the host is in progress, and transmission is possible up to the size of 0x7FFFF, but it cannot transmit more than that.
When referring to stm32f2xx_ll_usb.c, the maximum transfer size can be specified up to 0x7FFFF.
#define USB_OTG_DIEPTSIZ_XFRSIZ (0x7FFFFUL << 0U)
USBx_INEP(epnum)->DIEPTSIZ |= (USB_OTG_DIEPTSIZ_XFRSIZ & ep->xfer_len);
What should I do if I want to transmit more than 0x80000 data?
For example
Transmit data below 0x7FFFF -> Wait for transmission completion -> Transmit data below 0x7FFFF -> Wait for transmission completion -> ... -> Transmit the last data -> Wait for transmission completion -> Done
Is it possible to transmit only in this way?
Solved! Go to Solution.
2022-08-18 1:16 AM
> Is it possible to transmit only in this way?
Yes.
At the end of the day, the actual transfers happen in maxpacket sizes, anyway.
JW
2022-08-18 1:16 AM
> Is it possible to transmit only in this way?
Yes.
At the end of the day, the actual transfers happen in maxpacket sizes, anyway.
JW
2022-08-21 5:26 PM
Thank you for answer
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.