2022-06-20 10:18 AM
I'm working with the Nucleo-64 development board with an STM32L476 microcontroller and I'm using the USB source code that STM32CubeMX has generated for me. Every once in a while something unpredictable happens, e.g. the user unplugs the USB-cable in the middle of a packet or the microcontroller attempts to send something before the cable has been plugged in properly. When something goes wrong, I would like to have a reliable way to abort all ongoing transmissions/receptions and reset the USB state machine, without having to call __USB_FORCE_RESET or MX_USB_DEVICE_Init(). What would such a function look like? Right now I call these functions:
USB_FlushRxFifo(USB_OTG_FS);
USB_FlushTxFifo(USB_OTG_FS, 15);but I can see that ((USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData)->TxState is still 1 in some error cases. Can anybody please help me?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.