STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! If I want to use UCPD2 in STM32G0B1RCT6, is HSI16 the only choice as the driving clock for this integrated PD controller? May i use HSE?

In my application, UCPD2 will be active for USB type C PD Sink (45W), which will be working together with other peripherals, such as timers, USB(DEVICE), etc. If the driving clock for UCPD2 is HSI16(in datasheet described), if no other choice, that m...

0693W00000HoVNTQA3.png
Lmatt.11 by Associate III
  • 2687 Views
  • 3 replies
  • 0 kudos

Is there a simple way to use SDMMC1 an fatFS with NucleoH723 (I'm targetting H730 chip) polling or DMA

I try the code bellow an ST youtube video, about F7, sdmmc and fat FS, but it's not working.It seems to me there is no easy way about using SDMMC with H7.the DMA setting are to complicated for my knowledge, but maybe I am missing some point.Is there ...

Tbill.1 by Associate II
  • 1297 Views
  • 2 replies
  • 0 kudos

We found some time the UART interrupt call back function (HAL_UART_RxCpltCallback) will shut down but the IRQ function (UART5_IRQHandler ) still working. Because we have add the counter in call back function and IRQ function 。

We found some time the UART interrupt call back function (HAL_UART_RxCpltCallback) will shut down but the IRQ function (UART5_IRQHandler ) still working. Because we have add the counter in call back function and IRQ function , when the communication ...

User.100 by Associate II
  • 1885 Views
  • 3 replies
  • 0 kudos

SD Card and USB problems.

Hi, I'm working with an STM32F446VET MCU. The goal of the F446 is to get data from some sensors and store it on an SD Card and send it at the same time to a COM port. I was able to make Windows to recognize the USB/COM port (https://community.st.com/...

MBolo.1 by Associate III
  • 3204 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.