2017-07-17 1:28 PM
Posted on July 17, 2017 at 22:28
at the thread:
https://community.st.com/0D50X00009XkXXqSAN
I set the sd card as 4-bit width as mentioned on that thread. but cannot mount the sd card.
doe.john.016
suggest me use 1-bit width and the system could work well.
so my question is, why it couldn't work when I config the width as 4bit? how should I use the 4-bit sdio on F746?
2017-07-17 3:03 PM
You typically negotiate initial contact at low speed 1-bit, and then move to higher speeds and/or 4-bit if the card supports it by sending a command to the card, and switching modes on the SDIO controller side.
2017-08-03 1:45 PM
Thanks, that make me sense.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.