2022-12-26 12:32 PM
processing full erase cycle helps, but still have no idea, why device enters such condition!
Please help!
2023-01-02 8:35 AM
> openocd shows that device is protected
What is the state of Option Bytes, as read out by CubeProgrammer or similar, when this happens?
Do you reprogram portions of FLASH or option bytes in your program?
Does CubeProgrammer (or CubeIDE) run on the computer into which you connect the device, when this happens?
What is the normal setting of the Option Bytes and how is the pin related to starting the built-in bootloader (BOOT0) connected? (this question aims at the possible inadvertent running of the built-in bootloader)
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.