2022-03-24 6:50 AM
I have coded the function for the jump :
void vd_srv_BOOT_JumpToUserApp(uint32_t u32_AppAddr)
{
uint32_t temp = 0UL;
volatile uint32_t u32_JumpAddr = 0UL;
void (*pJumpToUserApp)(void) = (void*)0;
/* Disable MPU */
// HAL_MPU_Disable();
/* Disable HAL and HAL timer (TIM6) */
HAL_SuspendTick();
HAL_RCC_DeInit();
HAL_DeInit();
/* Disable interrupts for timers */
HAL_NVIC_DisableIRQ(SysTick_IRQn);
/* Clear any pending ones */
HAL_NVIC_ClearPendingIRQ(SysTick_IRQn);
/* Prepare jump address */
SCB->VTOR = (unsigned long)u32_AppAddr;
u32_JumpAddr = *(__IO uint32_t*) (u32_AppAddr + 4UL);
/* Prepare jumping function */
pJumpToUserApp = (void (*)(void)) u32_JumpAddr;
/* Initialize user application's stack pointer */
__set_MSP(*(__IO uint32_t*) u32_AppAddr);
/* Jump.*/
pJumpToUserApp();
}
The u32_AppAddr have the address 0x0800C000. and in the project that is placed at the address 0x0800C000, I have the *.ld file with :
MEMORY
{
CCMRAM (xrw) : ORIGIN = 0x10000000, LENGTH = 64K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K
FLASH (rx) : ORIGIN = 0x800C000, LENGTH = 976K
}
The function doesn't work. where is the problem?
2022-03-24 9:16 AM
Dont place VTOR change to bootloader code, right is app code system_xx
/*!< Uncomment the following line if you need to relocate your vector Table in
Internal SRAM. */
/* #define VECT_TAB_SRAM */
#define VECT_TAB_OFFSET 0xC000 /*!< Vector Table base offset field.
This value must be a multiple of 0x200. */
/******************************************************************************/
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.