2022-07-28 11:37 AM
Attempting to get USB CDC running on the CM4 core of a stock Nucleo-H745zi-q board. USB_CoreReset() times out waiting for a soft reset. Any help would be greatly appreciated.
Timeout is in stm32h7xx_ll_usb.c, lines 1456-1469:
/* Core Soft Reset */
count = 0U;
USBx->GRSTCTL |= USB_OTG_GRSTCTL_CSRST;
do
{
count++;
if (count > 200000U)
{
return HAL_TIMEOUT;
}
} while ((USBx->GRSTCTL & USB_OTG_GRSTCTL_CSRST) == USB_OTG_GRSTCTL_CSRST);USB clock is RC48
Project built with CubeMX V6.6.1, CubeIDE V1.10.1, Firmware FW_H7 V1.10.0
I moved the USB from the CM4 core to the CM7, and this issue does not occur.
Solved! Go to Solution.
2022-08-26 8:02 AM
Hello,
If you look at usbd_desc.c/line 337: Get_SerialNum() function does access the system memory. Unfortunately, CM4 doesn't have access to this region.
So to use the device ID as a serial number, you have to read it by CM7, save it in the RAM which will be available later-on for CM4.
You can test it by -in Get_SerialNum()- replacing:
deviceserial0 = *(uint32_t *) DEVICE_ID1;
deviceserial1 = *(uint32_t *) DEVICE_ID2;
deviceserial2 = *(uint32_t *) DEVICE_ID3;
by:
deviceserial0 = 0xABCDEF12;
deviceserial1 = 0x12345678;
deviceserial2 = 0x12A3D459;
2022-08-26 7:39 AM
Hello @WLear ,
You can refer to the following example provided under the H7 Firmware Package which uses both cores CM4 and CM7:
Path: Projects\STM32H747I-EVAL\Applications\USB_Device\HID-CM4_MSC-CM7
I hope this helps.
BeST Regards,
Walid
2022-08-26 8:02 AM
Hello,
If you look at usbd_desc.c/line 337: Get_SerialNum() function does access the system memory. Unfortunately, CM4 doesn't have access to this region.
So to use the device ID as a serial number, you have to read it by CM7, save it in the RAM which will be available later-on for CM4.
You can test it by -in Get_SerialNum()- replacing:
deviceserial0 = *(uint32_t *) DEVICE_ID1;
deviceserial1 = *(uint32_t *) DEVICE_ID2;
deviceserial2 = *(uint32_t *) DEVICE_ID3;
by:
deviceserial0 = 0xABCDEF12;
deviceserial1 = 0x12345678;
deviceserial2 = 0x12A3D459;
2022-08-26 8:42 AM
Thankyou. Unfortunately, this example exhibits the same issue as my code. See the response from @SofLit for the root cause.
2022-08-26 8:44 AM
Yes, This test patch does allow the USB init function to return without timing out. I trust this bug will be fixed in the next H7 firmware release.
2024-03-19 10:12 AM
I just ran into this bug, CubeIDE version 1.14.1, STM32H755, USB running on the CM4. Stepping through initialization I don't see it hitting the Get_SerialNum function before attempting the CoreReset. It times out waiting on USB_OTG_GRSTCTL_CSRST. I changed the Get_SerialNum function as described above but I'm still getting the time out. Were you able to implement a workaround to allow the CM4 to run USB? Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.