2025-01-15 1:09 PM
The USB_OTG_HS peripheral keeps timing out on init and hanging the whole program.
I have created a STM32 project using the NUCLEO-H7S3L8 board from the new project menu. I have enabled the USB_OTG_HS as device only (but left the middleware disabled) and written a simple blinky main. The code always times out on the "MX_USB_OTG_HS_PCD_Init". Specifically USB_CoreReset() times out in "stm32h7rsxx>USB_CoreInit". I have tried multiple different USB clock configurations (HSE, HSE/2 and PLL3Q) but it still times out.
Some people have suggested (Solved: STM32U595 timeout in USB_CoreReset() - STMicroelectronics Community) including the below in "HAL_PCD_MspInit" but STMCube cannot find it and I can't where to include it from
_HAL_RCC_SYSCFG_CLK_ENABLE();
I have included my project.zip but it is just the board default project. I have XSPI1, XSPI2 and ExternalMemLoader disabledExternal disabled., And have enabled the High-Speed Crystal/Ceramic Resonator, the blue LED and the USB_OTG_HS as device only.
I'm really struggling to find a way forward, I would appreciate any guidance.
2025-01-15 1:47 PM
> I have enabled the USB_OTG_HS as device only (but left the middleware disabled)
So just try to set it (in Cube) to the function, you want.
(I never tried : enable USB , but not setting it to do something)
On the NUCLEO-H7S3L8 i could try it next days...but not now. (No time now.)
2025-01-15 2:25 PM
If I set the function it still timeout at USB_CoreReset(). I'm trying to use TinyUSB instead of the STM32 USB Middleware so don't want to set the device function in the IOC.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.