2025-01-23 4:46 AM - last edited on 2025-01-23 4:57 AM by Andrew Neil
Originally a reply in this thread - split as a separate question.
Hello
My blocking mode is working with "HAL_UART_Receive(&huart4, temp, 1, 100);"
Nonblocking mode is not working
Can you suggest anything to check?
I have defined as said
/* USER CODE BEGIN 2 */
HAL_UART_Receive_IT(&huart4, temp, 1);
/* USER CODE END 2 */
and
/* USER CODE BEGIN 4 */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
HAL_UART_Receive_IT(&huart4, temp, 1);
HAL_UART_Transmit(&huart4, temp, 1, 100);
}
/* USER CODE END 4 */
Solved! Go to Solution.
2025-01-26 9:22 PM - edited 2025-01-26 9:24 PM
Andrew Sir,
Apologies from my side and its been my pleasure for your valuable feedbacks.
Actual Problem is my BOOT mode pin it was not connected properly to the ground, somehow I got wrong short-link which has case but no short-link inside.
Things are working perfectly fine. Again thanks
2025-01-26 9:23 PM - edited 2025-01-26 9:23 PM
Karl Sir,
Apologies from my side and its been my pleasure for your valuable feedbacks.
Actual Problem is my BOOT mode pin it was not connected properly to the ground, somehow I got wrong short-link which has case but no short-link inside.
Things are working perfectly fine. Again thanks
2025-01-26 9:25 PM
Saket Sir,
Apologies from my side and its been my pleasure for your valuable feedbacks.
Actual Problem is my BOOT mode pin it was not connected properly to the ground, somehow I got wrong short-link which has case but no short-link inside.
Things are working perfectly fine. Again thanks
2025-01-27 12:59 AM
@KaushikSTM32 everyone can see all replies - there's no need to repeat.
You can mention multiple users using @
2025-01-27 9:17 PM
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.