2023-10-16 11:41 PM
Hi,
I am using stm32wb55 mcu with freeRtos, I changed the timebase source time to TIM17 as recommended when using freeRTOS but I am facing unxpected behavior unless I use TIM17 as the source time base the HAL_Delay is not working and the uwTick is stack on zero until the freeRtos schedular starts.
What I noticed that I did not get the TIM17 interrupt until the OS starts what is not clear for me, I changed the timebase source so I can call the HAL functions which are using the DELAY before the freeRTOS starts.
Any Idea
BR
Basel
2023-10-17 12:13 PM
This is a known issue with FreeRTOS. Any function that creates a FreeRTOS task/mutex/queue/etc. and is called before osKernelStart() will disable interrupts. This includes the usual MX_FREERTOS_Init() function. So any code you have between MX_FREERTOS_Init() and osKernelStart() will run with interrupts disabled.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.