STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

task is not running after hard reset in freertos

hi,I make bootloader to switch the code between two bank starting at address 0x08000000.and two application starting at 0x08020000 and 0x08100000 respectively, when I individual run the code it work fine, but when I hard reset the code, it goes to bo...

ykn by Senior
  • 1181 Views
  • 0 replies
  • 0 kudos

How to fix the I2C slave issue with STM32G070? HAL_I2C_ListenCpltCallback, HAL_I2C_AddrCallback, HAL_I2C_SlaveRxCpltCallback, HAL_I2C_SlaveTxCpltCallback

Hi, I'm trying to setup a stm32g070kb (32pin) MCU as I2C slave by using CubeIDE.I would like to create a code which will work same as I2C Eeprom, but when I ask the stm32 (with another MCU) to return me a register or registers value, the returned reg...

0693W00000aJJ7hQAG.jpg 0693W00000aJJBPQA4.png
MrLKovacs by Associate II
  • 7381 Views
  • 8 replies
  • 0 kudos

STM32C0316-DK-Brisk-Demo STM32 Git Hot Spot

This post is a constructive feedback channel for the STM32C0316-DK Brisk demo project.Implemented Application Functions:Alternative IO Drivers which can coexist with HAL'sSTM32 Vdd and Temperature monitoringAnalog Keyboard (ADC, Debouncing)LEDs (puls...

S.Ma by Principal
  • 2492 Views
  • 2 replies
  • 3 kudos

G4 CAN: How to use with USB?

Hi! I'm in a conundrum, and am wondering if there are hacks around this. I'd like to use CAN on a a G4. And give it updatable firmware by USB. My options appear to be this:#1: Share a CAN Rx line with Boot 0 pin.#2 Share CAN Rx line with USP_DN.Are e...

DOCon.1 by Senior
  • 961 Views
  • 0 replies
  • 0 kudos

USB DFU bootloader : start from source.

Hello,I am trying to restart a STM32L072 into DFU bootloader mode (using STM32 LoRa Discovery kit) .The bootloader is working and I can use it to flash my firmware using a jumper between BOOT0 and VCC.Now I would like to enter bootloader from source....

Slan by Associate II
  • 3592 Views
  • 5 replies
  • 0 kudos

USB_CoreReset fails with a TIMEOUT error.

I am trying to run a USB HS example with external PHY on NUCLEO-F756ZG. As I count find example I have gone ahead and created code from scratch. I am using USB3300 external PHY. I have made the proper connection except for RST and +5V to the module b...

Jayesh2 by Associate II
  • 1147 Views
  • 0 replies
  • 0 kudos

STM32F407 USB FS (Device Mode) not recognized. "Unknown USB Device (Device Descriptor Request Failed)" Error!

I've seen many topics similar to my problem and went through their solutions but they didn't work for me so I'm asking here with details related to my problem. I've made a PCB and implemented USB 2 FS on it using STM32F407 PHY in device mode. here is...

0693W00000NskvSQAR.png 0693W00000NskwkQAB.png
AA.20 by Associate II
  • 6103 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.