2021-03-15 9:01 AM
"HAL_I2C_MemTxCpltCallback" is not executed when using 'HAL_I2C_Mem_Read_DMA' in STM32F407VE MCU of STM32Cube_FW_F4_V1.26.0 while is executed normally in the old version STM32Cube_FW_F4_V1.25.0. It seems that it runs "I2C_MemoryTransmit_TXE_BTF" onces and never goes to "HAL_I2C_MemTxCpltCallback".
Meanwhile, 'HAL_I2C_MemRxCpltCallback' is called normally in STM32Cube_FW_F4_V1.26.0.
2021-03-16 1:24 AM
Hello @HLuo.1 and welcome to the STM32 Community :)
Thanks for pointing out this issue.
I am checking it internally and I will come back to you with update.
Imen
2021-03-16 7:35 AM
Hi @HLuo.1,
I don't see the issue you described when I check the difference between the STM32CubeF4 packages V1.26.0 and V1.25.0.
Maybe you have an issue when using the BTF() APIs compared to the old releases.
I suggest, as a first step, to run the I2C example available in STM32CubeF4 MCU package and compare your own project/code and configuration to identify what is going wrong: \STM32Cube_FW_F4_V1.26.0\Projects\STM32F4-Discovery\Examples\I2C
Please keep me updated on your update.
Imen
2021-03-17 8:19 PM
I finally found that it is the problem fo the slave device MPU6050, which responses no acknowledge to the master for the DEVICE_RESET instruction though STM32Cube_FW_F4V 1.25.0 works fine.
http://luohanjie.com/2021-03-18/stm32-hal-i2c-memtxcpltcallback-problem.html
2021-03-18 5:11 AM
Thank you @HLuo.1 for posting your findings of this issue.
After an internal check to see the impact between the two versions of STM32CubeF4 v1.25.0 and v1.26.0:
There is no issue reproduced when running the test on a STM32F407-DISCO board with an external EEPROM @100Khz on I2C1/PB6/PB7 connection, and no strange behavior detected by the tests using the two MCU packages.
The "HAL_I2C_MemTxCpltCallback" callback is well executed from "I2C_MemoryTransmit_TXE_BTF" when HAL_I2C_EV_IRQHANDLER is called.
Can you please help us to reproduce the behavior you encountered, by giving us more details such as:
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.