2018-01-03 7:05 AM
I've been some months working on a Firmware for STM32L476VG. I've made a second version of my PCB adding more hardware as 6 MOSFET controlled from MCU.
The problem is with the MOSFET controlled from PE10, as seen in the code below when I put the declarations and initialization which is correct or that�s what I think because I�ve been using same type of declarations and initializations in more projects, then the running/debug has strange behavior. It goes thru the code until it finds:
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
Here sometimes jumps to memory position 0000 0000,
Other it gets stuck at startup_stm32l476xxx.s LoopForever(line 118) � here it gets because strange or unexpected ISR, I have to investigate more about this.
If I comment lines:
HAL_GPIO_WritePin(GPIOE,GPIO_PIN_10,
GPIO_PIN_RESET);
GPIO_InitStruct.
Pin
= GPIO_PIN_10;
GPIO_InitStruct.
Mode
= GPIO_MODE_OUTPUT_OD;
GPIO_InitStruct.
Pull
= GPIO_NOPULL;
GPIO_InitStruct.
Speed
=
GPIO_SPEED_LOW
;HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
All runs perfect, except PE10
void
MX_GPIO_Init(
void)
{
GPIO_InitTypeDef
GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
/*Configure GPIO pin : PE10->PWR_BLE*/
HAL_GPIO_WritePin(GPIOE,GPIO_PIN_10,
GPIO_PIN_RESET);
GPIO_InitStruct.
Pin
= GPIO_PIN_10;
GPIO_InitStruct.
Mode
= GPIO_MODE_OUTPUT_OD;
GPIO_InitStruct.
Pull
= GPIO_NOPULL;
GPIO_InitStruct.
Speed
=
GPIO_SPEED_LOW
;HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/*Configure GPIO pin : PE9->PWR_RS485*/
HAL_GPIO_WritePin(GPIOE,GPIO_PIN_9,
GPIO_PIN_RESET);
GPIO_InitStruct.
Pin
= GPIO_PIN_9;
GPIO_InitStruct.
Mode
= GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.
Pull
= GPIO_NOPULL;
GPIO_InitStruct.
Speed
= GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/*Configure GPIO pin : PE11->PWR_DRIV*/
HAL_GPIO_WritePin(GPIOE,GPIO_PIN_11,
GPIO_PIN_RESET);
GPIO_InitStruct.
Pin
= GPIO_PIN_11;
GPIO_InitStruct.
Mode
= GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.
Pull
= GPIO_NOPULL;
GPIO_InitStruct.
Speed
= GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/*Configure GPIO pin : PE12->PWR_DISP*/
HAL_GPIO_WritePin(GPIOE,GPIO_PIN_12,
GPIO_PIN_RESET);
GPIO_InitStruct.
Pin
= GPIO_PIN_12;
GPIO_InitStruct.
Mode
= GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.
Pull
= GPIO_NOPULL;
GPIO_InitStruct.
Speed
= GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/*Configure GPIO pin : PA11->PWR_SD*/
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_11,
GPIO_PIN_RESET);
GPIO_InitStruct.
Pin
= GPIO_PIN_11;
GPIO_InitStruct.
Mode
= GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.
Pull
= GPIO_NOPULL;
GPIO_InitStruct.
Speed
= GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pin : PE1->PWR_ETH*/
HAL_GPIO_WritePin(GPIOE,GPIO_PIN_1,
GPIO_PIN_RESET);
GPIO_InitStruct.
Pin
= GPIO_PIN_1;
GPIO_InitStruct.
Mode
= GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.
Pull
= GPIO_NOPULL;
GPIO_InitStruct.
Speed
= GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
}
So, anybody has faound same strange behaviour?
Thanks
#hal-gpio #stm32 #gnu #l4762018-01-03 7:27 AM
Can't this be hardware issue, related to power supply/ground? What do those MOSFETs switch?
JW
2018-01-03 7:34 AM
I would like to add that, Debugging in step by step mode I'm unable to recreate the error i go thru all the HAL and GPIO files and I'm able to continue with normal program.
2018-01-03 8:33 AM
Ji JW,
they will drive some LEDs, but the MOSFETSs are not soldered yet.
GLdL
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.