STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 - External interrupt PD4 (Only LL)

Posted on November 09, 2017 at 11:55Hi friend.I try create program working with external interrupt. And I have a problem. Interrupt never work....int8_t InitPin(void){LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOD); LL_APB2_GRP1_EnableClock(LL_A...

STM32F407 DAC Output (12Bit) Droning

Posted on November 08, 2017 at 11:21Hey guys,I have some problem with the output of my DAC and I hope you have some idea, what went wrong... Situation:    I am trying to play a WAV audio file with the DAC of my STM32F407VET. I use a double buffer, t...

STM32L4 Standard Peripheral Libraries

Posted on November 08, 2017 at 09:37Hello,  Are the Standard Peripheral Libraries available for L4 series? If not, maybe it is possible to use StdPeriph from e.g. F4? Register addresses are the same or not? Maybe there is some way to extract it fr...

Kaza K by Associate II
  • 4966 Views
  • 8 replies
  • 0 kudos

RTX Critical Sections

Posted on November 08, 2017 at 08:46Hi,I am trying to port a code that is working with FreeRTOS to RTX. The microcontroller is the same: STM32F4.The code uses critical sections. I have tried using the same implementation for the critical section for...

andrei by Associate II
  • 913 Views
  • 0 replies
  • 0 kudos

STM32L4 USB CDC (VCP) Max packet transfer

Posted on January 26, 2017 at 11:29On investigating the use of the USB device drivers provided for the STM32Lx series chips (CDC) I found an issue when trying to transfer a packet to the PC which is an exact multiple of 64 bytes. In such a case the ...

Ant M by Associate II
  • 1820 Views
  • 2 replies
  • 0 kudos

USB MSC device implementation on Sensortile

Posted on November 05, 2017 at 23:00Hi,I am trying to implement USB  mass storage device class on the Sensortile which uses STM32L476. I used the sample audio loop  app to verify that USB works fine. However, when I ported the MSC device functions f...

Bala K by Associate
  • 1172 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.