2025-03-26 5:15 AM - last edited on 2025-03-26 5:26 AM by mƎALLEm
I use it to see if R S T is present in 3-phase systems with F072 c8t6 processor. I have defined only R pin as interrupt, the other two are defined as input. When I write the code as below, I cannot check the status of R. I guess it is because of the version or the processor I cannot use HAL_GPIO_EXTI_Rising_Callback
CODE:
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
sPhase_t *rstPhase = &taskPeripheralUnits.phase;
if(GPIO_Pin == ioR_Pin)
{
if (HAL_GPIO_ReadPin(ioR_GPIO_Port, ioR_Pin))
{
rstPhase->ucRawPhaseData[ZERO][rstFACTOR_R_PHASE] = ACTIVE;
rstPhase->ucRawPhaseData[ZERO][rstFACTOR_S_PHASE] = HAL_GPIO_ReadPin(ioS_GPIO_Port, ioS_Pin);
rstPhase->ucRawPhaseData[ZERO][rstFACTOR_T_PHASE] = HAL_GPIO_ReadPin(ioT_GPIO_Port, ioT_Pin);
}
else
{
rstPhase->ucRawPhaseData[1u][rstFACTOR_R_PHASE] = PASSIVE;
stPhase->ucRawPhaseData[1u][rstFACTOR_S_PHASE] = HAL_GPIO_ReadPin(ioS_GPIO_Port, ioS_Pin);
rstPhase->ucRawPhaseData[1u][rstFACTOR_T_PHASE] = HAL_GPIO_ReadPin(ioT_GPIO_Port, ioT_Pin);
}
}
}
2025-03-26 5:28 AM
The hardware is capable to select raising or falling external interrupt edge or both. This is reflected in STM32CubeMX as well.
> I cannot check the status of R
You are reading the pin level with HAL_GPIO_ReadPin.
So, what unexpected behaviour exactly are you observing?
hth
KnarF
2025-03-26 5:29 AM
Hello,
The question is not clear. Could you please elaborate/reword?
Regarding HAL_GPIO_EXTI_Rising_Callback() it's not available on STM32F0 CubeHAL. HAL_GPIO_EXTI_Rising_Callback() is available on STM32F0 CubeHAL like what you shared in your post.
2025-03-26 5:34 AM
I check whether there are 3 phases according to the states of the RS and T pins, but here the value of R always comes as 0 1 0 1. In my code, when R is 0, I write a voltage error, but even though R = 0, the error is not entered.
2025-03-26 9:15 AM
> the value of R always comes as 0 1 0 1
That's what I would expect from a periodic signal.
KnarfB
2025-03-27 1:12 AM - last edited on 2025-03-27 1:15 AM by mƎALLEm
/*Code with U073*/
void HAL_GPIO_EXTI_Falling_Callback(uint16_t GPIO_Pin)
{
sPhase_t *rstPhase = &taskPeripheralUnits.phase;
if (GPIO_Pin == ioINPEXT_R_Pin)
{
rstPhase->ucRawPhaseData[1u][rstFACTOR_R_PHASE] = PASSIVE;
rstPhase->ucRawPhaseData[1u][rstFACTOR_S_PHASE] = HAL_GPIO_ReadPin(ioINP_S_GPIO_Port, ioINP_S_Pin);
rstPhase->ucRawPhaseData[1u][rstFACTOR_T_PHASE] = HAL_GPIO_ReadPin(ioINP_T_GPIO_Port, ioINP_T_Pin);
}
}
/*---------------------------------------------------------------------------------------------------------------------------*/
void HAL_GPIO_EXTI_Rising_Callback(uint16_t GPIO_Pin)
{
sPhase_t *rstPhase = &taskPeripheralUnits.phase;
if (GPIO_Pin == ioINPEXT_R_Pin)
{
rstPhase->ucRawPhaseData[ZERO][rstFACTOR_R_PHASE] = ACTIVE;
rstPhase->ucRawPhaseData[ZERO][rstFACTOR_S_PHASE] = HAL_GPIO_ReadPin(ioINP_S_GPIO_Port, ioINP_S_Pin);
rstPhase->ucRawPhaseData[ZERO][rstFACTOR_T_PHASE] = HAL_GPIO_ReadPin(ioINP_T_GPIO_Port, ioINP_T_Pin);
}
}
/*---------------------------------------------------------------------------------------------------------------------------*/
static void prvRstPhaseExistanceCtrl(void)
{
sPhase_t *rstPhase = &taskPeripheralUnits.phase;
static TickType_t xTickTimer;
uint8_t Rdetected, Sdetected, Tdetected;
uint8_t *ucPhases[rstPHASE_COUNT_TOTAL] = {&Rdetected, &Sdetected, &Tdetected};
for (int Idx = ZERO; Idx < rstPHASE_COUNT_TOTAL; Idx++)
{
if (!(rstPhase->ucRawPhaseData[0][Idx] & rstPhase->ucRawPhaseData[1][Idx]) )
{
*(ucPhases[Idx]) = ACTIVE;
}
else
{
*(ucPhases[Idx]) = PASSIVE;
}
}
if((Rdetected & Sdetected & Tdetected) == ACTIVE)
{
xTickTimer = xTaskCurrentTick;
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ALL_DETECTED;
}
else
{
taskPeripheralUnits.phase.sequenceStatus.ucSequence = rstPHASE_SEQUENCE_WRONG;
if (xTaskCurrentTick - xTickTimer > timeDELAY_RST_CONTROL)
{
if((Rdetected & Sdetected) == ACTIVE)
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_RS_DETECTED;
}
else if((Sdetected & Tdetected) == ACTIVE)
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ST_DETECTED;
}
else if((Tdetected & Rdetected) == ACTIVE)
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_RT_DETECTED;
}
else if(Rdetected == ACTIVE)
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_R_DETECTED;
}
else if(Sdetected == ACTIVE)
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_S_DETECTED;
}
else if(Tdetected == ACTIVE)
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_T_DETECTED;
}
else /* None of them Active */
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ALL_NOT_DETECTED;
}
}
else
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ALL_DETECTED;
}
}
}
/* Code with F072 */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
sPhase_t *rstPhase = &taskPeripheralUnits.phase;
if(GPIO_Pin == ioR_Pin)
{
if (HAL_GPIO_ReadPin(ioR_GPIO_Port, ioR_Pin) == GPIO_PIN_RESET)
{
rstPhase->ucRawPhaseData[ZERO][rstFACTOR_R_PHASE] = ACTIVE;
rstPhase->ucRawPhaseData[ZERO][rstFACTOR_S_PHASE] = HAL_GPIO_ReadPin(ioS_GPIO_Port, ioS_Pin);
rstPhase->ucRawPhaseData[ZERO][rstFACTOR_T_PHASE] = HAL_GPIO_ReadPin(ioT_GPIO_Port, ioT_Pin);
}
else
{
rstPhase->ucRawPhaseData[1u][rstFACTOR_R_PHASE] = PASSIVE;
rstPhase->ucRawPhaseData[1u][rstFACTOR_S_PHASE] = HAL_GPIO_ReadPin(ioS_GPIO_Port, ioS_Pin);
rstPhase->ucRawPhaseData[1u][rstFACTOR_T_PHASE] = HAL_GPIO_ReadPin(ioT_GPIO_Port, ioT_Pin);
}
}
}
/*---------------------------------------------------------------------------------------------------------------------------*/
static void prvRstPhaseExistanceCtrl(void)
{
sPhase_t *rstPhase = &taskPeripheralUnits.phase;
static TickType_t xTickTimer;
uint8_t Rdetected, Sdetected, Tdetected;
uint8_t *ucPhases[rstPHASE_COUNT_TOTAL] = {&Rdetected, &Sdetected, &Tdetected};
for (int Idx = ZERO; Idx < rstPHASE_COUNT_TOTAL; Idx++)
{
if (!(rstPhase->ucRawPhaseData[0][Idx] & rstPhase->ucRawPhaseData[1][Idx]) )
{
*(ucPhases[Idx]) = ACTIVE;
}
else
{
*(ucPhases[Idx]) = PASSIVE;
}
}
if((Rdetected & Sdetected & Tdetected) == ACTIVE)
{
xTickTimer = xTaskCurrentTick;
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ALL_DETECTED;
vSciPrintf((uint8_t *) "1\n");
}
else
{
taskPeripheralUnits.phase.sequenceStatus.ucSequence = rstPHASE_SEQUENCE_WRONG;
if (xTaskCurrentTick - xTickTimer > timeDELAY_RST_CONTROL)
{
if((Rdetected & Sdetected) == ACTIVE)
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_RS_DETECTED;
vSciPrintf((uint8_t *) "2\n");
}
else if((Sdetected & Tdetected) == ACTIVE)
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ST_DETECTED;
vSciPrintf((uint8_t *) "3\n");
}
else if((Tdetected & Rdetected) == ACTIVE)
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_RT_DETECTED;
vSciPrintf((uint8_t *) "4\n");
}
else if(Rdetected == ACTIVE)
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_R_DETECTED;
vSciPrintf((uint8_t *) "5\n");
}
else if(Sdetected == ACTIVE)
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_S_DETECTED;
vSciPrintf((uint8_t *) "6\n");
}
else if(Tdetected == ACTIVE)
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_T_DETECTED;
vSciPrintf((uint8_t *) "7\n");
}
else /* None of them Active */
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ALL_NOT_DETECTED;
vSciPrintf((uint8_t *) "8\n");
}
}
else
{
rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ALL_DETECTED;
}
}
}2025-03-27 1:14 AM
Hello,
Please use </> to share your code. I'm editing your post.
You can refer to this link on how to do it.
Thank you for your understanding.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.