2023-03-13 2:25 AM
Hi, I'm trying to practice FreeRTOS with my STM32F769I-Eval kit.
I made two task with different priority and print global variable with semaphore.
When I run my code, terminal print decreased value every time.
I don't know why. Here is my code.
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MPU Configuration--------------------------------------------------------*/
MPU_Config();
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART1_UART_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* USER CODE BEGIN RTOS_MUTEX */
/* add mutexes, ... */
/* USER CODE END RTOS_MUTEX */
/* Create the semaphores(s) */
/* definition and creation of mySemaphore */
osSemaphoreDef(mySemaphore);
mySemaphoreHandle = osSemaphoreCreate(osSemaphore(mySemaphore), 1);
/* USER CODE BEGIN RTOS_SEMAPHORES */
/* add semaphores, ... */
/* USER CODE END RTOS_SEMAPHORES */
/* USER CODE BEGIN RTOS_TIMERS */
/* start timers, add new ones, ... */
/* USER CODE END RTOS_TIMERS */
/* Create the queue(s) */
/* definition and creation of myQueue */
osMessageQDef(myQueue, 16, uint16_t);
myQueueHandle = osMessageCreate(osMessageQ(myQueue), NULL);
/* USER CODE BEGIN RTOS_QUEUES */
/* add queues, ... */
/* USER CODE END RTOS_QUEUES */
/* Create the thread(s) */
/* definition and creation of defaultTask */
// osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128);
// defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
/* definition and creation of myTestTask01 */
osThreadDef(myTestTask01, StartTask02, osPriorityLow, 0, 128);
myTestTask01Handle = osThreadCreate(osThread(myTestTask01), (void *)mySemaphoreHandle);
/* definition and creation of myTestTask02 */
osThreadDef(myTestTask02, StartTask03, osPriorityIdle, 0, 128);
myTestTask02Handle = osThreadCreate(osThread(myTestTask02), (void *)mySemaphoreHandle);
/* USER CODE BEGIN RTOS_THREADS */
/* add threads, ... */
/* USER CODE END RTOS_THREADS */
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}void StartTask02(void const * argument)
{
/* USER CODE BEGIN StartTask02 */
char buf[256];
osSemaphoreId semaphore = (osSemaphoreId)argument;
/* Infinite loop */
for(;;)
{
if(semaphore != NULL)
{
if(osSemaphoreWait(semaphore, osWaitForever) == osOK)
{
sprintf(buf, "Task02! : %d\r\n", g_iCount);
HAL_UART_Transmit(&huart1, (uint8_t*)buf, strlen(buf), 100);
osSemaphoreRelease(semaphore);
}
osDelay(500);
}
}
/* USER CODE END StartTask02 */
}
/* USER CODE BEGIN Header_StartTask03 */
/**
* @brief Function implementing the myTestTask02 thread.
* @param argument: Not used
* @retval None
*/
/* USER CODE END Header_StartTask03 */
void StartTask03(void const * argument)
{
/* USER CODE BEGIN StartTask03 */
char buf[256];
osSemaphoreId semaphore = (osSemaphoreId)argument;
/* Infinite loop */
for(;;)
{
if(semaphore != NULL)
{
if(osSemaphoreWait(semaphore, osWaitForever) == osOK)
{
sprintf(buf, "Task03! : %d\r\n", g_iCount);
HAL_UART_Transmit(&huart1, (uint8_t*)buf, strlen(buf), 100);
osSemaphoreRelease(semaphore);
}
osDelay(500);
}
}
/* USER CODE END StartTask03 */
}Please let me know why this starnge behavior happen.
Thanks.
Solved! Go to Solution.
2023-03-14 1:14 AM
The task stack size of only 128 is probably too small. Especially because you’re using printf-family functions usually requiring much more stack.
You really should enable FreeRTOS stack checking and define configASSERT for development.
2023-03-13 7:28 PM
Where is the rest of the code uses g_iCount?
2023-03-13 7:35 PM
Sorry, I didn't place my code. But I found the answer myself. I set the value to 0 in main instead out of main function.
__IO int g_iCount;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MPU_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
void StartDefaultTask(void const * argument);
void StartTask02(void const * argument);
void StartTask03(void const * argument);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MPU Configuration--------------------------------------------------------*/
MPU_Config();
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
g_iCount = 0;
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART1_UART_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* USER CODE BEGIN RTOS_MUTEX */
/* add mutexes, ... */
/* USER CODE END RTOS_MUTEX */
/* Create the semaphores(s) */
/* definition and creation of mySemaphore */
osSemaphoreDef(mySemaphore);
mySemaphoreHandle = osSemaphoreCreate(osSemaphore(mySemaphore), 1);
/* USER CODE BEGIN RTOS_SEMAPHORES */
/* add semaphores, ... */
/* USER CODE END RTOS_SEMAPHORES */
/* USER CODE BEGIN RTOS_TIMERS */
/* start timers, add new ones, ... */
/* USER CODE END RTOS_TIMERS */
/* Create the queue(s) */
/* definition and creation of myQueue */
osMessageQDef(myQueue, 16, uint16_t);
myQueueHandle = osMessageCreate(osMessageQ(myQueue), NULL);
/* USER CODE BEGIN RTOS_QUEUES */
/* add queues, ... */
/* USER CODE END RTOS_QUEUES */
/* Create the thread(s) */
/* definition and creation of defaultTask */
// osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128);
// defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
/* definition and creation of myTestTask01 */
osThreadDef(myTestTask01, StartTask02, osPriorityLow, 0, 128);
myTestTask01Handle = osThreadCreate(osThread(myTestTask01), (void *)mySemaphoreHandle);
/* definition and creation of myTestTask02 */
osThreadDef(myTestTask02, StartTask03, osPriorityIdle, 0, 128);
myTestTask02Handle = osThreadCreate(osThread(myTestTask02), (void *)mySemaphoreHandle);
/* USER CODE BEGIN RTOS_THREADS */
/* add threads, ... */
/* USER CODE END RTOS_THREADS */
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}After set the value in main function, It works correctly.
2023-03-14 1:14 AM
The task stack size of only 128 is probably too small. Especially because you’re using printf-family functions usually requiring much more stack.
You really should enable FreeRTOS stack checking and define configASSERT for development.
2023-03-14 1:37 AM
Thanks for reply.
I changed the buf size to 32, it works perfectly.
Your answer was really perfect!
Super Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.