STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 USB DFU bootloader not working reliably

I have a self powered STM32F446 with 24 MHz oscillator, not crystal. When trying to activate the bootloader mode, I get variable results. Sometimes it shows up properly, sometimes it shows up but in a corrupted type of state, and sometimes it doesn't...

Lee3 by Associate III
  • 3948 Views
  • 6 replies
  • 0 kudos

F411 USART LL Driver Not Work Well

I have made my own PCB board with F411 MCU.The USART2 does not work well if I use LL driver.This is the init code generated by CubeIDE.static void MX_USART2_UART_Init(void) {   /* USER CODE BEGIN USART2_Init 0 */   /* USER CODE END USART2_Init 0 ...

HDaji.1 by Senior
  • 1157 Views
  • 1 replies
  • 0 kudos

TCPP01-M12 appears to not be connecting CCx to CCxc

I am prototyping a new board upgrade to USB-C by connecting an X-Nucleo-SNK1M1 board containing the TCPP01-M12 to our existing USB device board that uses a STM32L476. The device is battery powered and will only need default 5V power. All that works...

RHinm.1 by Associate II
  • 5593 Views
  • 4 replies
  • 0 kudos

STM32F4xx USB Host BgndProcess

STM32F401in usbh_def.h:typedef struct { const char *Name; uint8_t ClassCode; USBH_StatusTypeDef(*Init)(struct _USBH_HandleTypeDef *phost); USBH_StatusTypeDef(*DeInit)(struct _USBH_HandleTypeDef *phost); USBH_StatusType...

TAzja.1 by Associate
  • 1353 Views
  • 1 replies
  • 0 kudos

I'm looking for a better way to make raw binary of signature & public key when I'm making a secure bootloader.

Hello, When I'm learning "STM32 security in practice MOOC". I ran into the below scripts to make raw binary of signature and public key. I thought it was not easy to use and explain to others. Is there a better way to make a raw binary of signature a...

eziya76 by Associate III
  • 4111 Views
  • 6 replies
  • 0 kudos

Resolved! Where is stsw-stm32054?

STM32F1x Standard Peripheral Library part number stsw-stm32054 does not appear.This library was released as V3.6.0 on November 05, 2021.I downloaded this library.However, it is currently unavailable. It seems that you can download the library from th...

HKim.27 by Associate
  • 4614 Views
  • 8 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.