2023-04-14 5:10 AM
Hi
I created a project from STM32CubeMX for the STM32F767ZI MCU:
After initialization, every task waits for message in its dedicated message queue. When the latest task blocks on reading its queue, a hard fault is generated:
The processor has escalated a configurable-priority exception to hardfault.
The HFSR.FORCED is set to 1.
The forced fault is not always the same. Here are the observed fault (for same code however !):
with PC=0x0 and LR=0x01
The exception is always raised after the following code (excerpt from xQueueReceive()):
if( xTaskResumeAll() == pdFALSE )
{
/* Set a PendSV to request a context switch. */
portNVIC_INT_CTRL_REG = portNVIC_PENDSVSET_BIT;
__DSB();
__ISB();
}The Idle task is never entered !
I have a limited knowledge of the Cortex M7 Interrupt system. I must dive into it. Meanwhile, how can I investigate such a problem ? Any support is welcome.
Thanks
Some more info about FreeRTOS config:
#define configENABLE_FPU 0
#define configENABLE_MPU 0
#define configUSE_PREEMPTION 1
#define configSUPPORT_STATIC_ALLOCATION 1
#define configSUPPORT_DYNAMIC_ALLOCATION 1
#define configUSE_IDLE_HOOK 1
#define configUSE_TICK_HOOK 0
#define configCPU_CLOCK_HZ ( SystemCoreClock )
#define configTICK_RATE_HZ ((TickType_t)1000)
#define configMAX_PRIORITIES ( 56 )
#define configMINIMAL_STACK_SIZE ((uint16_t)128)
#define configTOTAL_HEAP_SIZE ((size_t)15360)
#define configMAX_TASK_NAME_LEN ( 16 )
#define configUSE_TRACE_FACILITY 1
#define configUSE_16_BIT_TICKS 0
#define configIDLE_SHOULD_YIELD 0
#define configUSE_MUTEXES 1
#define configQUEUE_REGISTRY_SIZE 8
#define configUSE_RECURSIVE_MUTEXES 1
#define configUSE_COUNTING_SEMAPHORES 1
#define configUSE_PORT_OPTIMISED_TASK_SELECTION 0
#define configRECORD_STACK_HIGH_ADDRESS 1
Solved! Go to Solution.
2023-04-17 3:06 AM
Found the error : in the xPortPendSVHandler() call, I could observe that the LR register was set to a spurious value (0x00000001) while popping the core registers for the Idle task. From there, it was easy to identify a stack overflow issue.
Thanks to @Pavel A. and to @Community member for your support. Best regards
2023-04-14 6:28 AM
Do you use floating point? If so, define configENABLE_FPU 1
2023-04-14 6:38 AM
No use of floating point.
Thanks for this clarification.
2023-04-14 6:51 AM
On CM7 with DMA, watch for a) Cache Coherency and b) Life/Scope of buffer
Look if you use stack or auto/local variables for DMA buffers
Look at buffer alignment, caching is on 32-byte boundaries.
Use ByAddr cache management to limit action.
Avoid DCacheInvalidate unless necessary and watch for serious side-effects
2023-04-14 7:15 AM
Waw ! Thanks for all those points to check !
I did not look at the DMA side since any communication worked fine. I'll do and come back with more info ...
2023-04-14 8:17 AM
The 2 first points have been checked.
For the 2 last points, it is not clear to me. I need to look for some more info.
2023-04-14 8:20 AM
I temporarily avoid the hard fault by creating an additional task that is always active (endless loop). This plays the role of the Idle task.
What could prevent to use the default Idle task ?
2023-04-17 1:13 AM
Actually, where is the the "PendSV_Handler" defined ?
2023-04-17 1:22 AM
Forget this. Apologizes
2023-04-17 3:06 AM
Found the error : in the xPortPendSVHandler() call, I could observe that the LR register was set to a spurious value (0x00000001) while popping the core registers for the Idle task. From there, it was easy to identify a stack overflow issue.
Thanks to @Pavel A. and to @Community member for your support. Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.