2025-02-18 12:21 AM
Hello all,
I am using IAR Embedded Workbench 8.22.3 and needed to add support for the STM32G4 series (specifically the STM32G431RB). Since this version of IAR does not natively support STM32G4, I followed the official patch installation process.
When trying to Download and Debug, the following error appeared in the IAR Debug Log:
Checked the flash loader directory:
:file_folder: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0 EWARM F\S 8.22.3\arm\config\flashloader\ST\
Found the following files:
Tried selecting different loaders, but none worked.
Any insights or suggestions would be greatly appreciated. Thanks!
Solved! Go to Solution.
2025-05-20 4:07 AM
Hello @Umesh_Kumar278
Please find attached the old EWARM patch supporting STM32G431RB part numbers.
Note: There is no need to install this patch with the new EWARM version starting from V8.50, as it is already taken into consideration by the toolchain itself.
Regards,
2025-05-20 4:07 AM
Hello @Umesh_Kumar278
Please find attached the old EWARM patch supporting STM32G431RB part numbers.
Note: There is no need to install this patch with the new EWARM version starting from V8.50, as it is already taken into consideration by the toolchain itself.
Regards,
2025-05-26 3:26 AM
Hello @KORKAD ,
I tried the latest patch and modifying the .mac file. I managed to do that , and I will try with this patch as well.
Thanks and regards,
Umesh
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.